图为硬件连接 USB0_ID 浮空。和EVM板卡硬件连接差不多,软件用的TI Android JB-4.2.2-DevKit-4.1.1开发包,软件在开发板上面运行USB0 OTG没问题,但是在我自己做的板卡上面就出现插上USB线时候,PC识别为unkown device,串口无打印,当拔掉USB时候,提示musb android_usb gadget disconnected。个人感觉硬件和软件都没问题,但是USB0的OTG就是不通,USB1的HOST模式已经调通了。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
图为硬件连接 USB0_ID 浮空。和EVM板卡硬件连接差不多,软件用的TI Android JB-4.2.2-DevKit-4.1.1开发包,软件在开发板上面运行USB0 OTG没问题,但是在我自己做的板卡上面就出现插上USB线时候,PC识别为unkown device,串口无打印,当拔掉USB时候,提示musb android_usb gadget disconnected。个人感觉硬件和软件都没问题,但是USB0的OTG就是不通,USB1的HOST模式已经调通了。
我看了原理图,没发现什么问题
您可以查看下http://processors.wiki.ti.com/index.php/Android_ADB_Setup 驱动是否正确
问题找到了,应该是PCB板卡布局问题,我现在在板卡和电脑间接了个hub转接,USB设备就识别为full_speed设备,然后PC机就能识别板卡了。想请问下,软件上面能强制为full_speed设备吗,找不到地方修改。