This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: dsplib.ae674" contains ELF object files which are incompatible with the TI-COFF output file. Ensure you are using the proper library.

Part Number: TMS320C6748


我在编译工程的时候,提示如下错误,utils.lib工程我已经找到并修改了COFF格式编译出来,但是这个dsplib.ae674没有找到,在哪里下载该ccs工程的?

  • -lE:/workspace_v5_5/Demo/StarterWare/Library/Platform/Debug/Platform.lib -lE:/workspace_v5_5/Demo/StarterWare/Library/StarterWare/Drivers/Debug/drivers.lib -l"E:/workspace_v5_5\Demo/StarterWare/Library/StarterWare/SystemConfig/Debug/system_config.lib" -l"libc.a" -l"E:\BaiduNetdiskDownload\TL6748-EVM_V5.1\Demo\Algorithm\Library\DSPLib\dsplib.ae674" -l"E:\BaiduNetdiskDownload\TL6748-EVM_V5.1\Demo\Algorithm\Library\StarterWare\Utils\Debug\utils.lib"
    warning #10373-D: library "E:\BaiduNetdiskDownload\TL6748-EVM_V5.1\Demo\Algorithm\Library\DSPLib\dsplib.ae674" contains ELF object files which are incompatible with the TI-COFF output file. Ensure you are using the proper library.
    warning #10373-D: library "E:\BaiduNetdiskDownload\TL6748-EVM_V5.1\Demo\Algorithm\Library\StarterWare\Utils\Debug\utils.lib" contains ELF object files which are incompatible with the TI-COFF output file. Ensure you are using the proper library.
    warning #10373-D: library "E:\BaiduNetdiskDownload\TL6748-EVM_V5.1\Demo\Algorithm\Library\DSPLib\dsplib.ae674" contains ELF object files which are incompatible with the TI-COFF output file. Ensure you are using the proper library.
    warning #10373-D: library "E:\BaiduNetdiskDownload\TL6748-EVM_V5.1\Demo\Algorithm\Library\StarterWare\Utils\Debug\utils.lib" contains ELF object files which are incompatible with the TI-COFF output file. Ensure you are using the proper library.

  •  ELF 对象文件与 TI-COFF 输出文件不兼容