Part Number: SK-TDA4VM
我在Ubuntu 18.04LTS环境下安装Linux-SDK时,按照教程安装V08.06.01.03版本SDK时,进行Yocto build时出现问题
按照教程,我将"/ti-processor-sdk-linux-j7-evm-08_06_01_03","gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu","gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf"文件夹 安装到/opt下
当我执行
TOOLCHAIN_BASE=/opt MACHINE=j7-evm bitbake -k tisdk-default-image
时,报错如下,似乎是因为交叉编译的文件名称不正确?但我并没有正确的文件下载路径,请帮我解决该问题,谢谢!
ERROR: Unable to start bitbake server (None)
ERROR: Server log for this session (/opt/ti-processor-sdk-linux-j7-evm-08_06_01_03/yocto-build/build/bitbake-cookerdaemon.log):
--- Starting bitbake server pid 13393 at 2024-03-06 13:30:50.151241 ---
ERROR: Failed to obtain external Arm toolchain version: Execution of '/opt/gcc-arm-9.2-ti2020.01-armv5-x86_64-arm-none-linux-gnueabi/bin/arm-none-linux-gnueabi-gcc -v' failed: command not found
ERROR: Failed to obtain external Arm toolchain version: Execution of '/opt/gcc-arm-9.2-ti2020.01-armv5-x86_64-arm-none-linux-gnueabi/bin/arm-none-linux-gnueabi-gcc -v' failed: command not found
ERROR: Error: EXTERNAL_TOOLCHAIN path '/opt/gcc-arm-9.2-ti2020.01-armv5-x86_64-arm-none-linux-gnueabi' does not exist