This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2EG-17: 运行apps.out时,打印乱码

Part Number: TDA2EG-17


在运行apps.out时,出现了乱码的消息,以下是系统应用启动的log:

DRA722-GP ES2.1
Trying to boot from MMC1
*** Warning - bad CRC, using default environment
spl: falcon_args_file not set in environment, falling back to default
Booting Linux on physical CPU 0x0
Linux version 4.19.73 (rd22673@RD08) (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #9 PREEMPT Thu Feb 29 10:21:20 CST 2024
CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c53c7d
CPU: div instructions available: patching division code
CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
OF: fdt: Machine model: TI DRA718 EVM
bootconsole [earlycon0] enabled
============================================================
                        come in rootfs
============================================================
--------------------------------------
      start check lock
--------------------------------------
environment: line 35: echo: write error: Device or resource busy
ERROR: 77 file /sys/class/gpio/136 is not exist.
WARE :  used default dir /app/firm
INFO :  *.rsc file is exist, continue.
INFO :  Loading dra7-dsp1-fw.xe66
INFO :  Loading dra7-ipu2-fw.xem4
Loaded PowerVR consumer services.
Starting avm apps: 

============================================================
                /app/start_avm_app.sh 
============================================================

INFO : check data dir...
Filesystem                Size      Used Available Use% Mounted on
/dev/root               147.1M     46.3M     89.8M  34% /
devtmpfs                 90.7M         0     90.7M   0% /dev
tmpfs                   135.7M         0    135.7M   0% /dev/shm
tmpfs                   135.7M         0    135.7M   0% /tmp
tmpfs                   135.7M         0    135.7M   0% /run
tmpfs                   135.7M         0    135.7M   0% /var/run
/dev/mmcblk0p3          205.2M     89.0M    101.4M  47% /app
/dev/mmcblk0p4           14.2G     43.8M     13.4G   0% /data
current apps process pid 123
current eventhy process pid 144
current ui process pid 145
Starting syslogd: OK
Running sysctl: OK
Starting mdev... app_root=/app/release
[awtk-port/main_loop_linux.c|main_loop_init:134] 
 [HOST]  OSA: HOST Remote Log Shared Memory @ 0x9fd4f140
 [HOST]  OSA: DSP1 Remote Log Shared Memory @ 0x9fd769e0
 [HOST]  OSA: IPU2 Remote Log Shared Memory @ 0x9fe63da0
 [HOST] [HOST  ]      3.567528 s:  SYSTEM: System A15 Init in progress !!!
 [HOST] [IPU2  ] 
                    [HOST] [IPU2  ]  [HOST] [IPU2  ] @
[HOST] [IPU2  ] A
[HOST] [IPU2  ] 
 [HOST] [IPU2  ] 

 [HOST] [IPU2  ] 
 [HOST] [IPU2  ] 0@
 [HOST] [IPU2  ] -
 [HOST] [IPU2  ]
  [HOST] [IPU2  ] S++
 [HOST] [IPU2  ] @
 [HOST] [IPU2  ] 
 [HOST] [IPU2  ] {+
 [HOST] [IPU2  ] @
 [HOST] [IPU2  ] `

请问是什么情况导致这个问题?我该如何解决?

感谢!