我们公司正在使用DM3730的平台,目前正在开发DM8148的平台又以下几个问题和疑问:
1、DM3730是dvsdk,DM8148是dvrrdk,二者的区别很大,以前算法、app和server都在codec_engine里面,可是dvrrdk里面如何开发app、算法很不清楚,想要一些好的资料对此进行了解。
2、以前的3730的arm是A8,最高主频是1G,最高mips是2000,但是实际查看内核中的cpuinfo显示mips只有998。
3、DM8148我看了dvrrdk里面的所有uboot,arm-speed都只配置成了600M和720M,既然最高主频是1G,为什么不配置成1G?另外就是mips,数据手册说最高mips是2000,可是实际看了cpuinfo只有599。
4、两种处理器的mips都比数据手册说的差距太大了,这样势必会大大降低处理器的性能,为什么会这样。