各位好!有问题需要请教一下!
我用AM3354 SDK里的linux驱动spidev.c生成驱动模块,然后用/Documentation/spi里的spidev_test.c生成应用程序,运行时,提示如下:
spidev spi2.0: setup: unsupported mode bits 10
can't set spi mode: Invalid argument
Aborted
PS:#define SPI_3WIRE 0x10 /* SI/SO signals shared */
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位好!有问题需要请教一下!
我用AM3354 SDK里的linux驱动spidev.c生成驱动模块,然后用/Documentation/spi里的spidev_test.c生成应用程序,运行时,提示如下:
spidev spi2.0: setup: unsupported mode bits 10
can't set spi mode: Invalid argument
Aborted
PS:#define SPI_3WIRE 0x10 /* SI/SO signals shared */
这个三线SPI的设备,需要在同一数据根线上能同时做MOSI和MISO。目前335上数据线可以配成MOSI,或者MISO,但是同时做,实现三线SPI,应该还不能支持。在TRM24.2.3中,对数据线的description描述中:Can be configured as either input or output (MOSI or MISO)
请问您这个驱动是在哪个驱动文件里修改的?
我们的SPI总线配置是在spi-omap2-mcspi.c进行修改的,spidev.c只是某一个SPI设备的驱动。
(1)我只是想用spidev.c这个应用层程序去测试AM3354是否支持3-wire的SPI。
(2)我现在的开发需求如下:
a. 我有一个液晶屏,该LCD接口集成了3-wire的SPI,而该SPI接口是连接AM3354的,该SPI的作用是:在LCD显示之前需要对液晶屏上的驱动IC进行初始化;
b. 因此,我单独写一个初始化LCD驱动IC的SPI设备驱动,同时在board-am335xevm.c中添加如下代码:
static struct pinmux_config spi1_pin_mux[] = {
{"mcasp0_aclkx.spi1_sclk", OMAP_MUX_MODE3 | AM33XX_PULL_ENBL
| AM33XX_INPUT_EN},
{"mcasp0_fsx.spi1_d0", OMAP_MUX_MODE3 | AM33XX_PULL_ENBL
| AM33XX_PULL_UP | AM33XX_INPUT_EN},
{"mcasp0_axr0.spi1_d1", OMAP_MUX_MODE3 | AM33XX_PULL_ENBL
| AM33XX_INPUT_EN},
{"mcasp0_ahclkr.spi1_cs0", OMAP_MUX_MODE3 | AM33XX_PULL_ENBL
| AM33XX_PULL_UP | AM33XX_INPUT_EN},
{NULL, 0},
};
static struct spi_board_info xxx_spi1_slave_info[] = {
{
.modalias = "xxx_spi_init",
// .platform_data = &xxx_spi_info,
.max_speed_hz = 24000000,
.bus_num = 2,
.chip_select = 0,
.mode = SPI_3WIRE,
},
};
但是系统启动时打印信息:
spi spi2.0: setup: unsupported mode bits 10
(3)求指教,谢谢!
我看了下这部分的代码,首先drivers/spi/spidev.c这个是个通用的SPI设备的驱动程序哦,并不是应用程序。
另外.mode 这个参数应该设为:
#define SPI_MODE_0 (0|0)
#define SPI_MODE_1 (0|SPI_CPHA)
#define SPI_MODE_2 (SPI_CPOL|0)
#define SPI_MODE_3 (SPI_CPOL|SPI_CPHA)
当中的一个。
SPI_3WIRE应该通过应用层的IOCTL函数进行设置。
Jian Zhou 于 2015-3-3 12:11 发表了以下帖子 :
我看了下这部分的代码,首先drivers/spi/spidev.c这个是个通用的SPI设备的驱动程序哦,并不是应用程序。
=====》【回复】 抱歉!笔误,我之前已经了解到drivers/spi/spidev.c是个通用的SPI设备的驱动程序,既然是通用驱动程序,那么也可以用在我的案例上。我是通过documentation/spi/spidev_test.c生成应用程序测试的。
运行命令如下:spidev_test -3 (注:3表示--3wire SI/SO signals shared)
打印信息:spidev spi2.0: setup: unsupported mode bits 10
PS:#define SPI_3WIRE 0x10 /* SI/SO signals shared */
【回复】