This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BeagleBone AM335X 第二个网口不通的问题,求助。

Other Parts Discussed in Thread: SYSCONFIG

如题。
目前正在调试基于BeagleBone AM335X 公司画的板子,利用了RGMII的第二路网口。

使用的PHY芯片是AT8031 两个,分别连接到 AM335X 的 RGMII1 和 RGMII2。
目前 RGMII1 对应的 eth0 是通的,工作正常。RGMII2 对应的eth1始终无法调通。

根据TI官网的 CPSW Ethernet Dual EMac 配置正确的 DeviceTree(pinmux & dual_emac = <1>,见底部),打开了 VLAN 选项。
确定了cpsw.c 中 ALE_Control 寄存器地址的 ale_vlan_aware 位设置了。

详细情况:
现象1 : eth1 和我的电脑直连,从eth1ping通我的电脑,并用wireshark抓到了ping的请求和反馈。可反过来电脑ping eth1不通。PS.电脑百兆网口
现象2:强制使用ethtool设置网口工作模式为 100M ,autoneg off , fule duplex模式,通过eth1 无法ping通外界。
现象3:设置eth1 的IP地址,外界能够ping通eth1的IP,但是从 eth0 进入的!!!看上去eth0模拟了虚拟IP。

原理理解:
CPSW 仅仅只是一个MAC来管理两个 PHY,所以中间引入了一个 ALE(address lookup engine)来做片选哪个PHY的工作。这样来管理两个PHY,并正常工作。不确定我理解的对不,所以查阅了 ALE_Control 和 ale_vlan_aware 寄存器均正确。


参考1 , device tree 节选:
cpsw_default: cpsw_default {
                pinctrl-single,pins = <
                        /* Slave 1 */
                        /*0x110 (PIN_INPUT_PULLUP | MUX_MODE2)*/        /* rgmii1_rxerr.rgmii1_rxerr */
                        0x114 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)        /* rgmii1_txen.rgmii1_txen */
                        0x118 (PIN_INPUT_PULLUP | MUX_MODE2)        /* rgmii1_rxdv.rgmii1_rxdv */
                        0x11c (PIN_OUTPUT_PULLDOWN | MUX_MODE2)        /* rgmii1_txd3.rgmii1_txd3 */
                        0x120 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)        /* rgmii1_txd2.rgmii1_txd2 */
                        0x124 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)        /* rgmii1_txd1.rgmii1_txd1 */
                        0x128 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)        /* rgmii1_txd0.rgmii1_txd0 */
                        0x12c (PIN_INPUT_PULLUP | MUX_MODE2)        /* rgmii1_txclk.rgmii1_txclk */
                        0x130 (PIN_INPUT_PULLUP | MUX_MODE2)        /* rgmii1_rxclk.rgmii1_rxclk */
                        0x134 (PIN_INPUT_PULLUP | MUX_MODE2)        /* rgmii1_rxd3.rgmii1_rxd3 */
                        0x138 (PIN_INPUT_PULLUP | MUX_MODE2)        /* rgmii1_rxd2.rgmii1_rxd2 */
                        0x13c (PIN_INPUT_PULLUP | MUX_MODE2)        /* rgmii1_rxd1.rgmii1_rxd1 */
                        0x140 (PIN_INPUT_PULLUP | MUX_MODE2)        /* rgmii1_rxd0.rgmii1_rxd0 */


                        /* Slave 2 */
                        0x40 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)        /* gpmc_a0.rgmii2_tctl */
                        0x44 (PIN_INPUT_PULLDOWN | MUX_MODE2)        /* gpmc_a1.rgmii2_rctl */
                        0x48 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)        /* gpmc_a2.rgmii2_td3 */
                        0x4c (PIN_OUTPUT_PULLDOWN | MUX_MODE2)        /* gpmc_a3.rgmii2_td2 */
                        0x50 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)        /* gpmc_a4.rgmii2_td1 */
                        0x54 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)        /* gpmc_a5.rgmii2_td0 */
                        0x58 (PIN_OUTPUT_PULLDOWN | MUX_MODE2)        /* gpmc_a6.rgmii2_tclk */
                        0x5c (PIN_INPUT_PULLDOWN | MUX_MODE2)        /* gpmc_a7.rgmii2_rclk */
                        0x60 (PIN_INPUT_PULLDOWN | MUX_MODE2)        /* gpmc_a8.rgmii2_rd3 */
                        0x64 (PIN_INPUT_PULLDOWN | MUX_MODE2)        /* gpmc_a9.rgmii2_rd2 */
                        0x68 (PIN_INPUT_PULLDOWN | MUX_MODE2)        /* gpmc_a10.rgmii2_rd1 */
                        0x6c (PIN_INPUT_PULLDOWN | MUX_MODE2)        /* gpmc_a11.rgmii2_rd0 */

                >;
        };
......
......
&cpsw_emac0 {
        phy_id = <&davinci_mdio>, <0>;
        mac-address = [ 12 23 34 45 56 67 ];
        phy-mode = "rgmii";
        dual_emac_res_vlan = <0>;
};

&cpsw_emac1 {
        phy_id = <&davinci_mdio>, <1>;
        phy-mode = "rgmii";
        mac-address = [ 22 32 43 54 65 76 ];
        dual_emac_res_vlan = <0>;
};

&mac {
    pinctrl-names = "default", "sleep";
    pinctrl-0 = <&cpsw_default>;
    pinctrl-1 = <&cpsw_sleep>;
    dual_emac;
};

参考2, Dual Emac 配置方法,节选 AM335X Technical Reference:
14.3.2.10.2 Dual Mac Mode
When operating in dual mac mode the intention is to transfer packets between ports 0 and 1 and ports 0
and 2, but not between ports 1 and 2. Each CPGMAC_SL appears as a single MAC with no bridging
between MAC’s. Each CPGMAC_SL has at least one unique (not the same) mac address.
Dual mac mode is configured as described below:
• Set the ale_vlan_aware bit in the ALE_Control register. This bit configures the ALE to process in vlan
aware mode.The CPSW_3G vlan aware bit (vlan_aware in CPSW_Control) determines how packets
VLAN’s are processed on CPGMAC_SL egress and does not affect how the ALE processes packets or
the packet destination. The CPSW_3G vlan aware bit may be set or not as required (must be set if
VLAN’s are to exit the switch).
• Configure the Port 1 to Port 0 VLAN
Add a VLAN Table Entry with ports 0 and 1 as members (clear the flood masks).
Add a VLAN/Unicast Address Table Entry with the Port1/0 VLAN and a port number of 0. Packets
received on port 1 with this unicast address will be sent only to port 0 (egress). If multiple mac addresses
are desired for this port then multiple entries of this type may be configured.
• Configure the Port 2 to Port 0 VLAN
Add a VLAN Table Entry with ports 0 and 2 as members (clear the flood masks).
Add a VLAN/Unicast Address Table Entry with the Port2/0 VLAN and a port number of 0. Packets
received on port 2 with this unicast address will be sent only to port 0 (egress). If multiple mac addresses
are desired for this port then multiple entries of this type may be configured.
• Packets from the host (port 0) to ports 1 and 2 should be directed. If directed packets are not desired
then VLAN with addresses can be added for both destination ports.
• Select the dual mac mode on the port 0 FIFO by setting tx_in_sel[1:0] = 01 in P0_Tx_In_Ctl. The
intention of this mode is to allow packets from both ethernet ports to be written into the FIFO without
one port starving the other port.
• The priority levels may be configured such that packets received on port 1 egress on one CPDMA RX
channel while packets received on port 2 egress on a different CPDMA RX channel.

PS. 我照做了,也确认过没有问题。

参考3, TI 官网 CPSW Ethernet配置介绍:
http://processors.wiki.ti.com/index.php/AM335x_CPSW_(Ethernet)_Driver%27s_Guide#Dual_Standalone_EMAC_mode 
我照做了,其中使用的SDK比较老,基于 kernel v3.2 的,而最新的基于 kernel v3.12 是 sdk7.0,但是发现最后的并没有这个选项: Emac switch  。有其他建议么?

期待回复啊。有人有类似的经验么?AM335X 第二路网口调通过的同仁们。

  • am33xx_cpsw_init 后面的两个参数,应该是phy本身的地址,写成字符串的形式。

    这个加了吗

  • 具体能说明在哪个源文件么?我看其他帖子也经常提到这个接口。但我貌似没有找到对一个的地方,麻烦提示下,谢谢。

  • 请查看 arch/arm/mach-omap2/board-am335xevm.c

  • 我目前使用的Linux版本是 3.14 ,我grep 了一下 所有am33xx_cp开头的,只能找到这些。

    [philip@catonbj arm]$ grep -rn "am33xx_cp"
    Binary file mach-omap2/omap_hwmod_33xx_43xx_interconnect_data.o matches
    Binary file mach-omap2/omap_hwmod_43xx_data.o matches
    Binary file mach-omap2/omap_hwmod_33xx_data.o matches
    mach-omap2/omap_hwmod_43xx_data.c:484:  .slave          = &am33xx_cpgmac0_hwmod,
    mach-omap2/omap_hwmod_43xx_data.c:743:  &am33xx_cpgmac0__mdio,
    Binary file mach-omap2/built-in.o matches
    mach-omap2/omap_hwmod_33xx_43xx_interconnect_data.c:149:struct omap_hwmod_ocp_if am33xx_cpgmac0__mdio = {
    mach-omap2/omap_hwmod_33xx_43xx_interconnect_data.c:150:        .master         = &am33xx_cpgmac0_hwmod,
    mach-omap2/omap_hwmod_33xx_43xx_common_data.h:36:extern struct omap_hwmod_ocp_if am33xx_cpgmac0__mdio;
    mach-omap2/omap_hwmod_33xx_43xx_common_data.h:95:extern struct omap_hwmod am33xx_cpgmac0_hwmod;
    Binary file mach-omap2/omap_hwmod_33xx_43xx_ipblock_data.o matches
    mach-omap2/omap_hwmod_33xx_data.c:464:  .slave          = &am33xx_cpgmac0_hwmod,
    mach-omap2/omap_hwmod_33xx_data.c:631:  &am33xx_cpgmac0__mdio,
    mach-omap2/omap_hwmod_33xx_43xx_ipblock_data.c:316:static struct omap_hwmod_class_sysconfig am33xx_cpgmac_sysc = {
    mach-omap2/omap_hwmod_33xx_43xx_ipblock_data.c:327:static struct omap_hwmod_class am33xx_cpgmac0_hwmod_class = {
    mach-omap2/omap_hwmod_33xx_43xx_ipblock_data.c:329:     .sysc           = &am33xx_cpgmac_sysc,
    mach-omap2/omap_hwmod_33xx_43xx_ipblock_data.c:332:struct omap_hwmod am33xx_cpgmac0_hwmod = {
    mach-omap2/omap_hwmod_33xx_43xx_ipblock_data.c:334:     .class          = &am33xx_cpgmac0_hwmod_class,
    mach-omap2/omap_hwmod_33xx_43xx_ipblock_data.c:1376:    CLKCTRL(am33xx_cpgmac0_hwmod, AM33XX_CM_PER_CPGMAC0_CLKCTRL_OFFSET);
    mach-omap2/omap_hwmod_33xx_43xx_ipblock_data.c:1449:    CLKCTRL(am33xx_cpgmac0_hwmod, AM43XX_CM_PER_CPGMAC0_CLKCTRL_OFFSET);

     

    是否后续的Linux版本已经对整个框架有一些调整?

  • 您用的是ezsdk 7.0么

    那么应该修改下您的板子对应的dts文件, 可以参考 am335x-evmsk.dts 中的cpsw_emac1等的配置。

  • 可以先在u-boot下把第二个网口测一下,排除下硬件的嫌疑

  • Hi,Yaoming Qin:

    我后来使用了 EZSDK7.0 之后(Linux 3.12),基于BB板,所以根据 am335x-evmsk.dts  配置的 am335x-bone-common.dtsi 对应网口的部分:

    cpsw_default: cpsw_default {
       pinctrl-single,pins = <
        /* Slave 1 */
        0x114 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txen.rgmii1_tctl */
        0x118 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxdv.rgmii1_rctl */
        0x11c (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd3.rgmii1_td3 */
        0x120 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd2.rgmii1_td2 */
        0x124 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd1.rgmii1_td1 */
        0x128 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd0.rgmii1_td0 */
        0x12c (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txclk.rgmii1_tclk */
        0x130 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxclk.rgmii1_rclk */
        0x134 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd3.rgmii1_rd3 */
        0x138 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd2.rgmii1_rd2 */
        0x13c (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd1.rgmii1_rd1 */
        0x140 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd0.rgmii1_rd0 */

        /* Slave 2 */
        0x40 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a0.rgmii2_tctl */
        0x44 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* gpmc_a1.rgmii2_rctl */
        0x48 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a2.rgmii2_td3 */
        0x4c (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a3.rgmii2_td2 */
        0x50 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a4.rgmii2_td1 */
        0x54 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a5.rgmii2_td0 */
        0x58 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* gpmc_a6.rgmii2_tclk */
        0x5c (PIN_INPUT_PULLDOWN | MUX_MODE2) /* gpmc_a7.rgmii2_rclk */
        0x60 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* gpmc_a8.rgmii2_rd3 */
        0x64 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* gpmc_a9.rgmii2_rd2 */
        0x68 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* gpmc_a10.rgmii2_rd1 */
        0x6c (PIN_INPUT_PULLDOWN | MUX_MODE2) /* gpmc_a11.rgmii2_rd0 */
       >;
      };

      cpsw_sleep: cpsw_sleep {
       pinctrl-single,pins = <
        /* Slave 1 reset value */
        0x114 (PIN_INPUT_PULLDOWN | MUX_MODE7)
        0x118 (PIN_INPUT_PULLDOWN | MUX_MODE7)
        0x11c (PIN_INPUT_PULLDOWN | MUX_MODE7)
        0x120 (PIN_INPUT_PULLDOWN | MUX_MODE7)
        0x124 (PIN_INPUT_PULLDOWN | MUX_MODE7)
        0x128 (PIN_INPUT_PULLDOWN | MUX_MODE7)
        0x12c (PIN_INPUT_PULLDOWN | MUX_MODE7)
        0x130 (PIN_INPUT_PULLDOWN | MUX_MODE7)
        0x134 (PIN_INPUT_PULLDOWN | MUX_MODE7)
        0x138 (PIN_INPUT_PULLDOWN | MUX_MODE7)
        0x13c (PIN_INPUT_PULLDOWN | MUX_MODE7)
        0x140 (PIN_INPUT_PULLDOWN | MUX_MODE7)

        /* Slave 2 reset value*/
        0x40 (PIN_INPUT_PULLDOWN | MUX_MODE7)
        0x44 (PIN_INPUT_PULLDOWN | MUX_MODE7)
        0x48 (PIN_INPUT_PULLDOWN | MUX_MODE7)
        0x4c (PIN_INPUT_PULLDOWN | MUX_MODE7)
        0x50 (PIN_INPUT_PULLDOWN | MUX_MODE7)
        0x54 (PIN_INPUT_PULLDOWN | MUX_MODE7)
        0x58 (PIN_INPUT_PULLDOWN | MUX_MODE7)
        0x5c (PIN_INPUT_PULLDOWN | MUX_MODE7)
        0x60 (PIN_INPUT_PULLDOWN | MUX_MODE7)
        0x64 (PIN_INPUT_PULLDOWN | MUX_MODE7)
        0x68 (PIN_INPUT_PULLDOWN | MUX_MODE7)
        0x6c (PIN_INPUT_PULLDOWN | MUX_MODE7)
       >;
      };

    ...

    &mac {
     pinctrl-names = "default", "sleep";
     pinctrl-0 = <&cpsw_default>;
     pinctrl-1 = <&cpsw_sleep>;
     dual_emac;
    };

    &davinci_mdio {
     pinctrl-names = "default", "sleep";
     pinctrl-0 = <&davinci_mdio_default>;
     pinctrl-1 = <&davinci_mdio_sleep>;
    };

    &cpsw_emac0 {
     phy_id = <&davinci_mdio>, <0>;
     phy-mode = "rgmii";
    };

    &cpsw_emac1 {
     phy_id = <&davinci_mdio>, <1>;
     phy-mode = "rgmii";
    };

    ...

    现象:

    eth0 eth1 均有,ifconfig eth1 up并配置好IP(ETH0 ETH1同网段)之后,从第二个网口并不能ping通,但把eth0网口插上,两个IP均可ping通,第二个网口可有可无。两个IP的数据均从ETH0进出。ETH0 和 ETH1 配置不同网段的IP,则无法访问 ETH1 的IP了。

    值得一提的是,拔插两个网线都有如下打印:

    eth0

    [ 1632.098610] libphy: 4a101000.mdio:00 - Link is Up - 100/Full

    eth1

    [ 1632.098610] libphy: 4a101000.mdio:01 - Link is Up - 100/Full

    硬件上的图片如图,两块8031的网口芯片,分别对应两个网口,左边是ETH1,右边是ETH0.

     

     

  • 在Uboot中做过如下实验:

    在boardinit的地方,cpsw有两个slave,默认使用第一个网口,后把顺序交换了一下,从第二个网口能够ping通外面。硬件上参考evm板做的,应该问题不大。可能在软件/dts的配置上。

  • 我 eth1 無法 ping 通卡了3個月了,這問題還是沒解。只要是 sdk7以上,都是這樣....官方給我的解答是大部分客戶用的是sdk6,sdk8少人碰。

    關於dts,我在E2E有人 AR8035 可以通,只是沒問她的 phy 是在slave1 還是 slave 2,然後dts也只是跟我說 phi_id 修改 & phy mode 修改就好了。

    可我的還是不行,ˋ這位大俠有甚麼心得題示能給小弟我嗎? 感激不盡

  • 请问您后来的问题解决了吗?

  • 双网口的功能,最好参考下我们AM335x SKEVM的板级代码,SKEVM是支持双网口功能的。