各位大神,我最近在测试C6678的DDR3接口速率。我使用的DDR3芯片支持最大1600M的时钟,DSP的CPU主频设置为1.25GKZ。使用EDMA进行DSP和DDR3之间的数据搬移,按照理论值计算那传输速率应该是1600MHZ*64bit/8=12800MB/S。但是在我实际测试中,测得的速率只有6300MB/S。后来我又把DDR3的速率降到1333MHZ,结果测得的速率还是6300MB/S。给人的感觉是达到了传输速率的瓶颈,但是不知道限制速率的原因是那些因素。希望知道的大神能帮我指点一下,谢谢!