This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138---SYSLINK--共享内存组件使用问题求助



syslink版本:syslink_2_21_01_05,使用examples/ex04_sharedregion这个列子改进,列子中原有的共享区域是SR0,SR1,其中SR0是给IPC使用,SR1是用户使用,由于项目需要存放两段不同的数据,存放的时间以及存放的内容都不相同,并且要分开保存,但总的大小只有1M,于是将SR1大小修改,并加入SR2区域,将原有的8M空间分成了两个4M大小的空间,之后进行编译,编译成功,也生成了可执行文件,运行可执行文件也没有问题,但是在CCS5.5中打开dsp.cfg文件就会报出以下错误:

Description Resource Path Location Type
Cannot read property "base" from undefined Dsp.cfg /ex04shar/dsp Configuration Validation XDCTools Configuration Marker

但是编译又能通过,就很不明白这是什么原因,请TI的技术人员帮忙回答下,我应该怎样消除这个原因啊?这个是不是要到syslink下修改源代码配置,然后重新编译啊?如果是这样,应该看哪个资料啊??

以下是错误截图:

以下是双击错误后,指向错误位置的截图: