This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问BBB如何在Android下开通MMC2



static struct pinmux_config mmc2_pin_mux[] = {
{"gpmc_ad12.mmc2_dat0", OMAP_MUX_MODE3 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad13.mmc2_dat1", OMAP_MUX_MODE3 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad14.mmc2_dat2", OMAP_MUX_MODE3 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_ad15.mmc2_dat3", OMAP_MUX_MODE3 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_csn3.mmc2_cmd", OMAP_MUX_MODE3 | AM33XX_PIN_INPUT_PULLUP},
{"gpmc_clk.mmc2_clk", OMAP_MUX_MODE3 | AM33XX_PIN_INPUT_PULLUP},
{NULL, 0},
};

我在Linux下作了如下端口,不知道这样配置是否正确,Linux启动的终端打印返回值-110的错误,不知道为啥

.gpio_cd = -EINVAL,
.gpio_wp = -EINVAL,

请教下这两个端口是干啥用的?什么时候需要配置,什么时候可以不必配置?