This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ar8031到am335x的布线问题

Other Parts Discussed in Thread: TLK105

各位:

    我计划使用ar8031千兆方式连接am335x,参考ti提供的标准方式。由于没有搞过千兆网络,想在软件上配置成100M运行。我的问题是:

1、原理图,ar8031和am335x按照千兆方式连接,参考ti提供的设计。用RGMII模式。ar8031和接插件也是千兆模式。

2、代码上,是否可以直接将ar8031强行配置为100M模式运行

我想了解一下,按照RGMII模式接线的时候,跑100M,各信号脚的速率和时序是怎么样的(千兆的线路,跑百兆。是各信号线速度不变,只是通信所用的【时间】变短了,只用10%的时间  就可以满足100M了。还是各信号线速度按比例下来了)。在这种组合情况下,是否有什么需要特别注意的地方,主要是硬件设计和布线。