This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教:哪里能找到C6678 EMIF NOR-FLASH BOOT 的2级加载代码?

CCS里好像没找到.

  • 对6678而言,EMIF boot时是直接跳转到0x70000000的地址执行,二级加载需要写一个程序放在0x70000000处执行负责后续程序的加载,附件是论坛上的一个例子供参考。

    boot.asm
  • 看过了你的例子,程序好像只能boot单个核。Ti 有没有提供多核加载的二级加载代码?

    有些文档讲,C66x系列的ROM boot loader 可以直接实现多核的加载无需用户的干预,哪些boot方式被支持呢?是不是C6678 EMIF NOR-FLASH加载方式不被支持?

    有些文档提到mergebtbl.exe工具,好像是用来把多个核的代码合成为一个文件,但怎么在ccs中无法找到该工具呢?

    谢谢!

     

  • 你好,我已经实现了SPI NOR加载,我把多个bin存到NOR FLASH(已实现),上电时先从NOR正常加载并执行a程序,a程序根据外部条件选择从NOR加载相应的bin到DDR3(已实现),我现在的问题是怎么从DDR3开始执行程序,有没有类似的例程或相应的文档,谢谢!

    还有,是不是a程序需要bin格式,其他程序要用out格式?