This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6745 SPI boot setting issue



请教几个问题:

1、在sprabb1c第6章

Master Boot – Booting From a Slave Memory Device
To boot from a slave memory device connected to SPI or I2C peripherals, AIS (in binary format) can be
directly Flashed to the memory device.
For booting from a NOR Flash, a configuration word is required before AIS as shown in Figure 3. NOR
Flash should be connected to EMA_CS[2] of the EMIFA peripheral

    -----是不是说如果要从spi flash启动 必须要连接到EMA_CS[2],如果需要的话是哪个pin要连?

2、spi flash 的地址应该映射到哪个范围

本人菜鸟,请高手指教,多谢!