This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168板子采用MCFW框架采集数据时,出现挂起的情况



问题现象:

       自己做的板子,采用的是8168/67芯片,用的DVR_RDK 2.0,当采用MCFW搭建link来采集视频时,会不定时出现(不同板子出现问题的时间频度也不一样)采集部分挂起的情况,经过分析发现挂起的位置是在MCFW的某个link里面,对MCFW框架未做过裁剪,不知道有人遇到过类似问题否? 已经折腾一阵了,还未定位和解决该问题。求助,多谢! 不知道是否DVRRDK2.x的版本有类似bug?

      主要核运行频率如下:

DSP clk: 987MHz

ARM clk: 987MHz

DDR clk: 675MHz

HDVICP clk: 600MHz
L3 Fast clk: 560MHz
HDVPSS clk: 280MHz
Ducati M3 clk: 280MHz