This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问如何降低BBB开发板的MMC2的CLK?



我看文件TI_Android_JB_4.2.2_DevKit_4.1.1/kernel/arch/arm/mach-omap2/clock33xx_data.c中MMC2的CLK设置如下

static struct clk mmc_clk = {
    .name       = "mmc_clk",
    .parent     = &per_192mhz_clk,
    .ops        = &clkops_null,
    .fixed_div  = 2,
    .recalc     = &omap_fixed_divisor_recalc,
};

static struct clk mmc2_ick = {
    .name       = "mmc2_ick",
    .parent     = &l4ls_gclk,
    .ops        = &clkops_null,
    .recalc     = &followparent_recalc,
};

static struct clk mmc2_fck = {
    .name       = "mmc2_fck",
    .clkdm_name = "l3s_clkdm",
    .parent     = &mmc_clk,
    .enable_reg = AM33XX_CM_PER_MMC2_CLKCTRL,
    .enable_bit = AM33XX_MODULEMODE_SWCTRL,
    .ops        = &clkops_omap2_dflt,
    .recalc     = &followparent_recalc,
};

也就是192/2=96MHz

我现在接一个WIFI设备无法工作,想尝试降低MMC2的频率到48MHz 或 24MHz,不知道是否可以在不影响MMC0和MMC2 的情况下实现?该怎么实现?

多谢指导

  • 问题补充:

    我示波器测出来mmc2_clk的波形为48MHz的正弦波

    是否可以把频率降低为24MHz?是否可以改为方波?

  • 请您查看 

    18.2.2 MMCHS Clock and Reset Management
    The MMCHS controller has separate bus interface and functional clocks. The debounce clock is created
    by dividing the 96-MHz (48 MHz @ OPP50) clock in the PRCM by two and then dividing the resulting 48-
    MHz (24 MHz @ OPP50) clock by a fixed 732.4219 (366.2109 @ OPP50) in the Control Module to get a
    32-kHz clock. This clock is fed back into the PRCM for clock gating. (See the CLK32KDIVRATIO_CTRL
    register in Chapter 9, Control Module, for more details).

    所以,需要把CPU降频,可以参考 http://processors.wiki.ti.com/index.php/AM335x_Power_Management_User_Guide#Static_CORE_OPP_50

    如果排除掉PCB layout的问题,我不觉得这个是需要降频解决的问题

  • MMC这部分的PCB布线是比价重要的,要注意信号线的等长,长度,以及上拉电阻的位置,如果用降低时钟的方法来debug硬件,可以修改MMC的相关驱动:

    \drivers\mmc\host\omap_hsmmc.c

    其中omap_hsmmc_set_clock()函数是设置时钟的。