Hi,
Thanks for help answer following question,
1、If a 10G-T1 PHY is connected to pcie,how connect the MDI interface of 10G-T1 PHY to DRA829?
2、There is only one MDI interface for CPSW 9 ethernet port,if phy address is not enough,how to connect the MDI of these PHY?
3、There is no PRU_ICSSG0 and PRU_ICSSG1 for DRV829V and DRV829J,does it mean I can't configure 4 RGMII to PRU_ICSSG interface?
4、How many RGMII interface I can configure at most for DRV829J?