CPU使用的是AM3354,现在遇到如下问题,当TPS65217C的外部输入电源出现虚连的情况时,65217会进入保护状态,无输出,即使输入电源稳定后,对65217进行复位,也不能恢复系统启动,除非重新上电,请问这个是什么情况,怎么解决。(正常启动后一切正常,问题只发生在用手连接输入电源,出现虚连时)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
手动连接输入电源并且出现虚接是什么意思?是指TPS65217的5V输入这里,出现虚接?手动控制这个5V输入情况?
是的,可以考虑为电源开关接触时抖动比较大,但是抖动后,能够可靠连接。
了解,这是个TPS65217输入端电源质量引起的电源芯片无法正常工作问题,和处理器本身没关系。你有在电源这个输入端加上去耦电容吗?有助于优化输入端的电源质量。
如果还是有那种TPS65217被保护的情况,建议你可以把这种问题发到我们论坛的电源板块,电源板块的专家们应该会有些好建议的。