This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

佐臻-TI-dm3730模块 UBIFS error (pid 1): ubifs_check_node:

Other Parts Discussed in Thread: DM3730

大家好,我使用佐臻的 DM3730 模块,我使用ANDROID 2.3.4系统,这个模块佐臻自己封装的,把DDRAM FALSH CPU都封装在一起,我两年前买的模块没有问题,但近期买的模块使用一段时间(有的是第一次烧录就出现)就出现UBIFS错误,相同的烧录文件,两年前买的就就没这个错误,使用很长时间也不出现UBIFS错误,新模块就出现了,从外观上模块的LOGO也是不一样的。大家有新的烧录命令吗? 我查看很多帖子,都说是制作UBIFS文件的命令不对,我的命令是这样的

$BOOT_NAND_TOOLS/mkfs.ubifs -r $BOOT_NAND_ROOTFS/ -m 2048 -e 126976 -c 3991 -o ubifs.img

$BOOT_NAND_TOOLS/ubinize -o $ANDROID_IMG/ubi.img -O 2048 -m 2048 -p 128KiB -s 512 $BOOT_NAND_TOOLS/ubinize.cfg

我的是sram 512M  FLASH 512M。

大家有合适的制作UBIFS文件的命令吗?

系统UBIFS损坏的部分LOG如下

GTP-INFO->>[528]Get the same mask version and same pid.
[    6.457427] <<-GTP-INFO->>[542]Don't meet the third condition.
[    6.463500] <<-GTP-ERROR->>[958]Load header file data failed!
[    6.469482] <<-GTP-DEBUG->> [1124]Update failed!
[    7.717987] UBIFS: recovery needed
[    7.823974] UBIFS error (pid 1): ubifs_check_node: bad CRC: calculated 0x7a9afaf1, read 0x884fd26c
[    7.833312] UBIFS error (pid 1): ubifs_check_node: bad node at LEB 1710:0
[    7.840393] UBIFS error (pid 1): ubifs_scanned_corruption: corruption at LEB 1710:0
[    7.853881] UBIFS error (pid 1): ubifs_recover_leb: LEB 1710 scanning failed
[    7.861938] VFS: Cannot open root device "ubi0:rootfs" or unknown-block(0,0)
[    7.869323] Please append a correct "root=" boot option; here are the available partitions:
[    7.878051] 1f00             512 mtdblock0  (driver?)
[    7.883300] 1f01            1280 mtdblock1  (driver?)
[    7.888580] 1f02             768 mtdblock2  (driver?)
[    7.893859] 1f03            5120 mtdblock3  (driver?)
[    7.899108] 1f04          516608 mtdblock4  (driver?)
[    7.904388] b300         3872256 mmcblk0  driver: mmcblk
[    7.909942]   b301           72261 mmcblk0p1 00000000-0000-0000-0000-000000000000mmcblk0p1
[    7.918548]   b302         1935832 mmcblk0p2 00000000-0000-0000-0000-000000000000mmcblk0p2
[    7.927154]   b303         1863540 mmcblk0p3 00000000-0000-0000-0000-000000000000mmcblk0p