This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

系统启动



你好:

   我用的8168的板子,EZSDK5.05的代码。把内存加大到2G。

1:  我该如何查看我板子上的内存是否有2G。

2:  我在系统启动时系统卡死在

Phy Addr : 0x48180d14 Data : 0x00000007
PRCM for IVHD1 is Done Successfully
PRCM for IVHD2 is in Progress, Please wait.....
BW Phy Addr : 0x48180800 Data : 0x00000002
AW Phy Addr : 0x48180800 Data : 0x00000002
Phy Addr : 0x48180e04 Data : 0x00000037
BW Phy Addr : 0x48180820 Data : 0x00070000
AW Phy Addr : 0x48180820 Data : 0x00050002
BW Phy Addr : 0x48180824 Data : 0x00030000
AW Phy Addr : 0x48180824 Data : 0x00010002
Phy Addr : 0x48180800 Data : 0x00000102
BW Phy Addr : 0x48180e10 Data : 0x00000007
AW Phy Addr : 0x48180e10 Data : 0x00000003
Phy Addr : 0x48180e14 Data : 0x00000004
BW Phy Addr : 0x53088000 Data : 0x10438ffc
AW Phy Addr : 0x53088000 Data : 0xeafffffe
BW Phy Addr : 0x53098000 Data : 0x080736d1
AW Phy Addr : 0x53098000 Data : 0xeafffffe
BW Phy Addr : 0x48180e10 Data : 0x00000003
AW Phy Addr : 0x48180e10 Data : 0x00000000
Phy Addr : 0x48180e14 Data : 0x00000007
PRCM for IVHD2 is Done Successfully
PRCM Initialization completed

这里跑不下去该如何解决。谢谢!

  • 建议先从硬件上确认你的8168板子是否贴了2GB的内存,从DDR的颗粒信息上可以读到。

  • 你好:

       1: 板子上确认是贴的2G内存,我该如何在系统里确认,系统是否认到了2G内存。

       2: 关于你上面说的从DDR的颗粒信息上可以看到。这个可以说的详细一下吗?如何看DDR颗粒信息。

     

    谢谢!

  •    1: 板子上确认是贴的2G内存,我该如何在系统里确认,系统是否认到了2G内存。

    -- 系统里面没法读出或者确认所接内存的容量,但是可以通过LISA寄存器配置情况来确认系统是否有将2GB的物理内存映射到系统里面。可以参考下面的wiki:

    http://processors.wiki.ti.com/index.php/EZSDK_Memory_Map

       2: 关于你上面说的从DDR的颗粒信息上可以看到。这个可以说的详细一下吗?如何看DDR颗粒信息。

    -- 一般的DDR颗粒的P/N带有的信息可以通过其Datasheet来解读。