各位好:
我们的板子是基于AM335Xboneblack制作的,一个是去除eeprom的我按照TI工程师提供的方法去除部门代码后程序到这边就结束了,我也没有修改任何
uart的代码。
[ 0.294036] io scheduler cfq registered (default)
[ 0.296264] Could not set LED4 to fully on
[ 0.299560] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
还有一个我们移植好的eeprom但是我也同样删除了代码,系统却能正常启动。两个板子还有一个差别就是第一个板子的DDR3是我重新配置的。