去年做的AM335X的主板,电源芯片用的是TPS65217C,配的是AM3352+128DDR3,刚开始回来的时候上电,发现回来的20块板子,只有1块能正常启动,主板将LDO2连接LED灯,上电后,LED灯一直闪烁;
问题一,通过全面检查,最后怀疑是TPS65217C芯片的BAT引脚悬空造成的,焊接104电容后,板子基本都能启动,但是将电池的对地电容换成105及以上,主板就无法启动了,这个是为什么?
问题二,按设计是在系统输入5V电源,需要PB_IN按键拉低系统才能起来,5V一上电,系统就直接起来了?
问题三,起来的板子在调试过程中,无意中就出来起不来现象,断电后检查发现TPS65217C的LDO4的3.3V和DCDC3的VCORE短路,TPS65217C电源正常,开始调试时候出现3块,没有太注意,今天他们在测试时有出现2块同样的问题,我们觉得这个问题比较严重。不知道这个问题怎么解决,是啥原因造成的,要不然我们后面不敢进行批量呀。