千兆网没使用PHY,采用mac_mac_forcedlink强制链接。
1:对serdes和sgmii的配置与例子配置一样(该例子是在DSP上运行并能进行千兆网通信),PA时钟和SGMII时钟也设置相同
This is SGMII config
mr_adv_ability is: 00009801
control is: 00000020
mask is: 00000001
2:使用port0端口,在Mac_CTL寄存器值为0(其地址为:0x02090904.例子程序值为0x008400a1)--这个寄存器的值存在不通,但是修改了写入0x008400a1值后,memory browser显示还是0
3:在ping过程中,keystone2_eth_rcv_packet函数对hd变量一直是NULL(网线的连接是好的)
对于以上背景,uboot下ping不通PC,请问这是怎么回事?十万火急············