This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

omapl138 arm中开启cache导致spi flash读写错误



如果不开cache,spi flash没有问题;开cache后,发现写进flash的数据和回读数据不一致。

cache开启流程如下:

    MMUTtbInit();

    // Configures translation table base register
    // with pagetable base address.
    CP15TtbSet((UINT)m_auiPageTable);

    // Enables MMU
    CP15MMUEnable();

    // Enable Instruction Cache
    CP15ICacheEnable();

    // Enable Data Cache
    CP15DCacheEnable();

是否是cache使用有误?

  • 有无将SPI访问的地址空间加入到可cache的表中?

  • 我把所有代码段和数据段全部都加入到cache表了:

    #define CACHE_DDR_START_ADDR                0xC00         // 0xC0000000
    #define CACHE_DDR_END_ADDR                  0xC10         // 0xC1000000

    static void MMUTtbInit(void)
    {

     UINT   uiIdx;


        for (uiIdx = 0; uiIdx < (4*1024); uiIdx++)
        {
            if ((uiIdx >= CACHE_DDR_START_ADDR) && (uiIdx < CACHE_DDR_END_ADDR))
            {
             m_auiPageTable[uiIdx] = (uiIdx << 20) | 0x00000C1E;
            }

            else
            {
             m_auiPageTable[uiIdx] = (uiIdx << 20) | 0x00000C12;
            }
        }

    }