大家好!
自己根据TI做的开发板,但是启动的时候遇到问题了,大家帮忙看看!谢谢
[ 0.000000] Linux version 3.2.0 (haungkun@huangkun) (gcc version 4.7.3 201304
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instructie
[ 0.000000] Machine: am335xevm
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM335X ES2.1 (sgx neon )
[ 0.000000] ------------[ cut here ]------------
[ 0.000000] WARNING: at arch/arm/mach-omap2/clkt_clksel.c:194 omap2_clksel_r)
[ 0.000000] clock: Could not find fieldval 0 for clock dpll_core_m6_ck parenk
[ 0.000000] Modules linked in:
[ 0.000000] Backtrace:
[ 0.000000] [<c0017dbc>] (dump_backtrace+0x0/0x10c) from [<c0414430>] (dump_)
[ 0.000000] r6:c0030acc r5:00000009 r4:c05d5e78 r3:c05f80cc
[ 0.000000] [<c0414418>] (dump_stack+0x0/0x1c) from [<c003f250>] (warn_slowp)
[ 0.000000] [<c003f1fc>] (warn_slowpath_common+0x0/0x6c) from [<c003f30c>] ()
[ 0.000000] r8:80000200 r7:c06541a4 r6:00000000 r5:c05e8c38 r4:00000000
[ 0.000000] r3:00000009
[ 0.000000] [<c003f2d4>] (warn_slowpath_fmt+0x0/0x40) from [<c0030acc>] (oma)
[ 0.000000] r3:00000000 r2:c05023d4
[ 0.000000] [<c0030a04>] (omap2_clksel_recalc+0x0/0x134) from [<c00357e0>] ()
[ 0.000000] r6:c06541dc r5:c05e8b38 r4:c05e8c38
[ 0.000000] [<c00357ac>] (propagate_rate+0x0/0x54) from [<c00357ec>] (propag)
[ 0.000000] r5:c05e8adc r4:c05e8b24
[ 0.000000] [<c00357ac>] (propagate_rate+0x0/0x54) from [<c00357ec>] (propag)
[ 0.000000] r5:c05e8a24 r4:c05e8ac8
[ 0.000000] [<c00357ac>] (propagate_rate+0x0/0x54) from [<c00357ec>] (propag)
[ 0.000000] r5:c05e8910 r4:c05e8a10
[ 0.000000] [<c00357ac>] (propagate_rate+0x0/0x54) from [<c0035950>] (recalc)
[ 0.000000] r5:c05f783c r4:c05e88fc
[ 0.000000] [<c0035910>] (recalculate_root_clocks+0x0/0x58) from [<c05a6bd8>)
[ 0.000000] r5:c05e878c r4:c05e878c
[ 0.000000] [<c05a6b54>] (am33xx_clk_init+0x0/0xa0) from [<c05a6920>] (omap3)
[ 0.000000] r5:c0a6f040 r4:00003517
[ 0.000000] [<c05a6840>] (omap3xxx_clk_init+0x0/0x314) from [<c05a05b8>] (am)
[ 0.000000] r7:c06541a4 r6:c06541dc r5:c0a6f040 r4:c05c6538
[ 0.000000] [<c05a057c>] (am33xx_init_early+0x0/0x40) from [<c059cde0>] (set)
[ 0.000000] [<c059c6cc>] (setup_arch+0x0/0x804) from [<c05995a4>] (start_ker)
[ 0.000000] [<c059952c>] (start_kernel+0x0/0x2dc) from [<80008040>] (0x80008)
[ 0.000000] r6:c05c79b8 r5:c05d6084 r4:10c53c7d
[ 0.000000] ---[ end trace 1b75b31a2719ed1c ]---
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pa8
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 e
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 512MB = 512MB total
[ 0.000000] Memory: 513168k/513168k available, 11120k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0599000 (5700 kB)
[ 0.000000] .init : 0xc0599000 - 0xc05d4000 ( 236 kB)
[ 0.000000] .data : 0xc05d4000 - 0xc063e730 ( 426 kB)
[ 0.000000] .bss : 0xc063e754 - 0xc066d524 ( 188 kB)
[ 0.000000] NR_IRQS:396
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrus
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 1s
[ 0.000000] Console: colour dummy device 80x30
[ 0.000305] Calibrating delay loop... 298.59 BogoMIPS (lpj=1492992)
[ 0.067626] pid_max: default: 32768 minimum: 301
[ 0.067901] Security Framework initialized
[ 0.068084] Mount-cache hash table entries: 512
[ 0.068786] CPU: Testing write buffer coherency: ok
[ 0.096405] omap_hwmod: pruss: failed to hardreset
[ 0.098663] print_constraints: dummy:
[ 0.099395] NET: Registered protocol family 16
[ 0.103881] OMAP GPIO hardware version 0.1
[ 0.109741] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.113861] omap_i2c.1: alias fck already exists
[ 0.115692] omap2_mcspi.1: alias fck already exists
[ 0.116210] omap2_mcspi.2: alias fck already exists
[ 0.118377] edma.0: alias fck already exists
[ 0.118438] edma.0: alias fck already exists
[ 0.118469] edma.0: alias fck already exists
[ 0.180877] bio: create slab <bio-0> at 0
[ 0.185638] SCSI subsystem initialized
[ 0.189147] usbcore: registered new interface driver usbfs
[ 0.189819] usbcore: registered new interface driver hub
[ 0.190216] usbcore: registered new device driver usb
[ 0.190826] registerd cppi-dma Intr @ IRQ 17
[ 0.190856] Cppi41 Init Done Qmgr-base(e087a000) dma-base(e0878000)
[ 0.190887] Cppi41 Init Done
[ 0.190917] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
[ 0.191558] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
[ 0.194030] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[ 0.197052] tps65910 1-002d: could not be detected
[ 0.200103] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 0.202423] Switching to clocksource gp timer
[ 0.238220] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 0.238525] musb-hdrc musb-hdrc.0: dma type: dma-cppi41
[ 0.239196] MUSB0 controller's USBSS revision = 4ea20800
[ 0.239288] musb0: Enabled SW babble control
[ 0.241271] musb-hdrc musb-hdrc.0: USB OTG mode controller at e083c000 using8
[ 0.241607] musb-hdrc musb-hdrc.1: dma type: dma-cppi41
[ 0.242248] MUSB1 controller's USBSS revision = 4ea20800
[ 0.242309] musb1: Enabled SW babble control
[ 0.243347] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 0.243499] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus numb1
[ 0.243774] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.243804] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber1
[ 0.243835] usb usb1: Product: MUSB HDRC host driver
[ 0.243835] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd
[ 0.243865] usb usb1: SerialNumber: musb-hdrc.1
[ 0.245727] hub 1-0:1.0: USB hub found
[ 0.245788] hub 1-0:1.0: 1 port detected
[ 0.247009] musb-hdrc musb-hdrc.1: USB Host mode controller at e083e800 usin9
[ 0.247833] NET: Registered protocol family 2
[ 0.248168] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.248748] TCP established hash table entries: 16384 (order: 5, 131072 byte)
[ 0.249481] TCP bind hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.249877] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.249908] TCP reno registered
[ 0.249938] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.250000] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.250427] NET: Registered protocol family 1
[ 0.250976] RPC: Registered named UNIX socket transport module.
[ 0.251007] RPC: Registered udp transport module.
[ 0.251007] RPC: Registered tcp transport module.
[ 0.251037] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.251495] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.282653] VFS: Disk quotas dquot_6.5.2
[ 0.282775] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.283874] msgmni has been set to 1002
[ 0.290283] alg: No test for stdrng (krng)
[ 0.291534] io scheduler noop registered
[ 0.291564] io scheduler deadline registered
[ 0.291687] io scheduler cfq registered (default)
[ 0.294006] Could not set LED4 to fully on
[ 0.297180] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[ 1.117980] console [ttyO0] enabled
[ 1.123138] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 1.131561] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 1.139953] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 1.148345] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 1.156707] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 1.166076] omap4_rng omap4_rng: OMAP4 Random Number Generator ver. 2.00
[ 1.194274] brd: module loaded
[ 1.208831] loop: module loaded
[ 1.212554] i2c-core: driver [tsl2550] using legacy suspend method
[ 1.219177] i2c-core: driver [tsl2550] using legacy resume method
[ 1.225769] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.293121] No daughter card found
[ 1.296813] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.312225] AM335X: wrong header 0xffffffff, expected 0xee3355aa
[ 1.318634] The error message above indicates that there is an issue with
[ 1.318634] the EEPROM or the EEPROM contents. After verifying the EEPROM
[ 1.318664] contents, if any, refer to the am335x_evm_setup function in the
[ 1.318695] arch/arm/mach-omap2/board-am335xevm.c file to modify the board
[ 1.318695] initialization code to match the hardware configuration
CTRL-A Z for help |115200 8N1 | NOR | Minicom 2.5 | VT102 | Online 00:01