This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6748 EDMA 通过MCASP的DA输出过程问题。

在编写AD/DA后进行测试,发现AD已经跑通,可是DA没有反应。

第一个问题是音频信号在CODEC的输出地址是0X01D02000与LINE IN 口一个地址,该如何理解?

第二个问题是DA输出的PING-PONG PARAM已经设定好了,与AD除地址和TCC外无异(AD已经跑通),但没有反应,为何?

(附MCASP AD\DA配置程序)

    mcasp_rx_i2s_activate();
    mcasp_tx_i2s_activate();
/*
 * McASP transmit config as i2s mode
 */
void mcasp_rx_i2s_config(void)
{
    /* Set I2S format in the receiver format units */
    McASPRxFmtI2SSet(SOC_MCASP_0_CTRL_REGS, WORD_SIZE, SLOT_SIZE,
                     MCASP_RX_MODE_DMA);

    /* Configure the frame sync. I2S shall work in TDM format with 2 slots */
    McASPRxFrameSyncCfg(SOC_MCASP_0_CTRL_REGS, 2, MCASP_RX_FS_WIDTH_WORD,
                        MCASP_RX_FS_EXT_BEGIN_ON_FALL_EDGE);

    /* configure the clock for receiver */
    McASPRxClkCfg(SOC_MCASP_0_CTRL_REGS, MCASP_RX_CLK_EXTERNAL, 0, 0);
    McASPRxClkPolaritySet(SOC_MCASP_0_CTRL_REGS, MCASP_RX_CLK_POL_RIS_EDGE);
    McASPRxClkCheckConfig(SOC_MCASP_0_CTRL_REGS, MCASP_RX_CLKCHCK_DIV32,
                          0x00, 0xFF);

    /* Enable the receiver slots. I2S uses 2 slots */
    McASPRxTimeSlotSet(SOC_MCASP_0_CTRL_REGS, I2S_SLOTS);

    /*
    ** Set the serializers, Currently only one serializer is set as
    ** transmitter and one serializer as receiver.
    */
    McASPSerializerRxSet(SOC_MCASP_0_CTRL_REGS, MCASP_XSER_RX);
}

/*
 * McASP recieve config as i2s mode
 */
void mcasp_tx_i2s_config(void)
{
  /* Set I2S format in the transmitter format units */
    McASPTxFmtI2SSet(SOC_MCASP_0_CTRL_REGS, WORD_SIZE, SLOT_SIZE,
                     MCASP_TX_MODE_DMA);

    /* Configure the frame sync. I2S shall work in TDM format with 2 slots */
    McASPTxFrameSyncCfg(SOC_MCASP_0_CTRL_REGS, 2, MCASP_TX_FS_WIDTH_WORD,
                         MCASP_TX_FS_EXT_BEGIN_ON_RIS_EDGE);

    /* configure the clock for transmitter */
 McASPTxClkCfg(SOC_MCASP_0_CTRL_REGS, MCASP_TX_CLK_EXTERNAL, 0, 0);
 McASPTxClkPolaritySet(SOC_MCASP_0_CTRL_REGS, MCASP_TX_CLK_POL_FALL_EDGE);
 McASPTxClkCheckConfig(SOC_MCASP_0_CTRL_REGS, MCASP_TX_CLKCHCK_DIV32,
       0x00, 0xFF);

    /* Enable the transmit slots. I2S uses 2 slots */
    McASPTxTimeSlotSet(SOC_MCASP_0_CTRL_REGS, I2S_SLOTS);

 /*
 ** Set the serializers, Currently only one serializer is set as
 ** transmitter and one serializer as receiver.
 */
 McASPSerializerTxSet(SOC_MCASP_0_CTRL_REGS, MCASP_XSER_TX);
}

/*
** Activates the data transmission/reception
** The DMA parameters shall be ready before calling this function.
*/
void mcasp_tx_i2s_activate(void)
{
    /* Start the clocks */
    McASPTxClkStart(SOC_MCASP_0_CTRL_REGS, MCASP_TX_CLK_EXTERNAL);

    /* Activate the  serializers */
    McASPTxSerActivate(SOC_MCASP_0_CTRL_REGS);

//    /* make sure that the XDATA bit is cleared to zero */
//    while(McASPTxStatusGet(SOC_MCASP_0_CTRL_REGS) & MCASP_TX_STAT_DATAREADY);

    /* Activate the state machines */
    McASPTxEnable(SOC_MCASP_0_CTRL_REGS);
}

/*
** Activates the data recieve
** The DMA parameters shall be ready before calling this function.
*/
void mcasp_rx_i2s_activate(void)
{
    /* Start the clocks */
    McASPRxClkStart(SOC_MCASP_0_CTRL_REGS, MCASP_RX_CLK_EXTERNAL);

    /* Activate the  serializers */
    McASPRxSerActivate(SOC_MCASP_0_CTRL_REGS);

    /* Activate the state machines */
    McASPRxEnable(SOC_MCASP_0_CTRL_REGS);
}

 

  • void aic31_adc_config(void)
    {
        /* enable the programmable PGA for left and right ADC  */
     codec_reg_write(AIC31_P0_REG15, 0x00);
     codec_reg_write(AIC31_P0_REG16, 0x00);

        /* MIC3L/R is not connected to the left ADC PGA */
     codec_reg_write(AIC31_P0_REG17, 0xFF);

        /* MIC3L/R is not connected to the right ADC PGA */
     codec_reg_write(AIC31_P0_REG18, 0xFF);

        /* power on the Line L1R */
     codec_reg_write(AIC31_P0_REG19, 0x04);

        /* power on the Line LIL */
     codec_reg_write(AIC31_P0_REG22, 0x04);
    }

    /**
     * \brief   Initializes the DAC section of the AIC31 Codec
     *
     * \param   baseAddr     Base Address of the interface connected to AIC31
     *
     * \return  None.
     *
     **/
    void aic31_dac_config(void)
    {
        /* power up the left and right DACs */
     codec_reg_write(AIC31_P0_REG37, 0xE0);

        /* select the DAC L1 R1 Paths */
     codec_reg_write(AIC31_P0_REG41, 0x02);
     codec_reg_write(AIC31_P0_REG42, 0x6C);


        /* DAC L to HPLOUT Is connected */
     codec_reg_write(AIC31_P0_REG47, 0x80);
     codec_reg_write(AIC31_P0_REG51, 0x09);

        /* DAC R to HPROUT is connected */
     codec_reg_write(AIC31_P0_REG64, 0x80);
     codec_reg_write(AIC31_P0_REG65, 0x09);

        /* DACL1 connected to LINE1 LOUT */
     codec_reg_write(AIC31_P0_REG82, 0x80);
     codec_reg_write(AIC31_P0_REG86, 0x09);

        /* DACR1 connected to LINE1 ROUT */
     codec_reg_write(AIC31_P0_REG92, 0x80);
     codec_reg_write(AIC31_P0_REG93, 0x09);

        /* unmute the DAC */
     codec_reg_write(AIC31_P0_REG43, 0x00);
     codec_reg_write(AIC31_P0_REG44, 0x00);
    }

    DAC部分的HPLOUT与HPROUT 好像与RIGHT_LOP/M及left_LOP/M重复了。二者选哪一个?

  •  0x01d02000处输出为此,让人不解,是DA配错了吗?

  • 调DA的时候可以先用示波器看一下从DSP的 MCASP数据输出引脚上看一下有没有数据出来。

  • 好的,我尝试尝试