This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ffmpeg解码支持

Other Parts Discussed in Thread: AM3358

我们在对讲的时候,视频通过ffmpeg解码之后,要用opengl来渲染,在调用glGenTextures的时候获取的都是0。

请问如果我要使用opengl,内核里面还需要在添加什么配置吗?

有没有相关资源可以支持下。谢谢。

  • 你是想用内部的3D加速模块,还是不用的?E2E论坛上有个帖子讨论Building OpenGL on the AM335x EVM,参考一下:

    http://e2e.ti.com/support/arm/sitara_arm/f/791/t/342126

  • 执行make BUILD=release OMAPES=8.x all_km的时候报错了:

     1:make: *** /home/lltang/Graphics_SDK_5_01_01_02/graphics/Graphics_SDK_5_01_01_02/GFX_Linux_KM: 没有那个文件或目录。 停止。

    2:/home/lltang/Graphics_SDK_5_01_01_02/GFX_Linux_KM/services4/srvkm/env/linux/module.c:51:42: fatal error: linux/platform_data/sgx-omap.h: 没有那个文件或目录

  • 你有正常安装过graphic SDK吗?应该是有这个目录和文件的。如果有的话,请注意路径的设置是否正确。

  • 安装过的。需要copy什么文件么?

    1, 修改了Rules.make 的GFX_KERNMOD_SRCPATH

    这个问题好了。

    2,我注释了头文件,编译过了。

    不过出现下面问题。

     root@am335x-evm:/mnt/nfs# insmod pvrsrvkm.ko
    Disabling lock debugging due to kernel taint
    root@am335x-evm:/mnt/nfs# insmod omaplfb.ko 
    Unable to handle kernel NULL pointer dereference at virtual address 00000000
    pgd = ce120000
    [00000000] *pgd=8e4ec831, *pte=00000000, *ppte=00000000
    Internal error: Oops: 17 [#1]
    Modules linked in: omaplfb(O+) pvrsrvkm(O)
    CPU: 0    Tainted: G           O  (3.2.0-gd53561e-dirty #112)
    PC is at AllocateDeviceID+0xc/0x54 [pvrsrvkm]
    LR is at PVRSRVRegisterDCDeviceKM+0xfc/0x188 [pvrsrvkm]
    pc : [<bf006d2c>]    lr : [<bf00299c>]    psr: 40000013
    sp : ce0f1e40  ip : ce0f1e50  fp : ce0f1e4c
    r10: 00177000  r9 : 00000000  r8 : 00000000
    r7 : ce1a787c  r6 : 00000000  r5 : ce1a7804  r4 : 00000000
    r3 : ce202e80  r2 : 00000001  r1 : ce202e88  r0 : 00000000
    Flags: nZcv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user
    Control: 10c5387d  Table: 8e120019  DAC: 00000015
    Process insmod (pid: 1387, stack limit = 0xce0f02f0)
    Stack: (0xce0f1e40 to 0xce0f2000)
    1e40: ce0f1e74 ce0f1e50 bf00299c bf006d2c ce512d00 ce202e80 ce1a7800 00000000
    1e60: 00000000 00177000 ce0f1eac ce0f1e78 bf037e1c bf0028ac c07eb1e0 c07eb1e0
    1e80: 00000000 d09e1000 bf038fec 00000001 bf039034 ce512d80 00000001 bf03b000
    1ea0: ce0f1ebc ce0f1eb0 bf03b010 bf037a20 ce0f1efc ce0f1ec0 c0008690 bf03b00c
    1ec0: ce0f1eec bf038fec 00000001 bf039034 ce512d80 bf038fec 00000001 bf039034
    1ee0: ce512d80 00000001 c0063df4 0000001c ce0f1fa4 ce0f1f00 c0066520 c0008600
    1f00: bf038ff8 c0019644 00000000 c0063eec 00000000 c03fa690 00000001 c054b170
    1f20: 00000000 00000000 00000000 00000000 00000000 00000000 d09e1000 00007fbe
    1f40: d09e659c d09e6463 d09e87cc ce202e80 00002128 00002738 00000000 00000000
    1f60: 0000001e 0000001f 0000000f 0000000d 0000000c 00000000 00000002 40264b08
    1f80: 00000000 00021d90 00000080 c0013ae8 ce0f0000 00000000 00000000 ce0f1fa8
    1fa0: c0013940 c0064e30 40264b08 00000000 400c5000 00007fbe 4017b230 00000002
    1fc0: 40264b08 00000000 00021d90 00000080 000210b0 00007fbe 4017b230 00000000
    1fe0: 402145a0 beb80ad8 40173b24 402145b0 80000010 400c5000 00000000 00000000
    Backtrace: 
    [<bf006d20>] (AllocateDeviceID+0x0/0x54 [pvrsrvkm]) from [<bf00299c>] (PVRSRVRegisterDCDeviceKM+0xfc/0x188 [pvrsrvkm])
    [<bf0028a0>] (PVRSRVRegisterDCDeviceKM+0x0/0x188 [pvrsrvkm]) from [<bf037e1c>] (OMAPLFBInit+0x408/0x5a0 [omaplfb])
     r7:00177000 r6:00000000 r5:00000000 r4:ce1a7800
    [<bf037a14>] (OMAPLFBInit+0x0/0x5a0 [omaplfb]) from [<bf03b010>] (OMAPLFB_Init+0x10/0x34 [omaplfb])
    [<bf03b000>] (OMAPLFB_Init+0x0/0x34 [omaplfb]) from [<c0008690>] (do_one_initcall+0x9c/0x16c)
    [<c00085f4>] (do_one_initcall+0x0/0x16c) from [<c0066520>] (sys_init_module+0x16fc/0x1884)
    [<c0064e24>] (sys_init_module+0x0/0x1884) from [<c0013940>] (ret_fast_syscall+0x0/0x30)
    Code: e89da830 e1a0c00d e92dd800 e24cb004 (e5902000) 
    ---[ end trace 39e43c85a5b1ea1c ]---
    Segmentation fault
  • 按照网上我重新编译了,发现如下问题。请问可能是什么原因?

    root@am335x-evm:~# /etc/init.d/335x-demo
    0x10205
    debug8.x
    /dev/mem opened.
    Memory mapped at address 0x40166000.
    Read at address  0x44E0007C (0x4016607c): 0x00030000
    Write at address 0x44E0007C (0x4016607c): 0x00000002, readback 0x00000002
    installing 8.x SGX debug user libraries

    Installing PowerVR Consumer/Embedded DDK 'sgxddk_1.10@2359475' on target

    File system installation root is /

    Uninstalling existing version sgxddk_1.10@2359475
    Uninstallation completed.
    boot script rc.pvr -> /etc/init.d/rc.pvr
    kernel module pvrsrvkm.ko -> /lib/modules/3.2.0-gd53561e-dirty/extra/pvrsrvkm.ko
    kernel module omaplfb.ko -> /lib/modules/3.2.0-gd53561e-dirty/extra/omaplfb.ko
    shared library libGLES_CM.so -> /usr/lib/libGLES_CM.so.1.10.2359475
    shared library libusc.so -> /usr/lib/libusc.so.1.10.2359475
    shared library libGLESv2.so -> /usr/lib/libGLESv2.so.1.10.2359475
    shared library libglslcompiler.so -> /usr/lib/libglslcompiler.so.1.10.2359475
    shared library libIMGegl.so -> /usr/lib/libIMGegl.so.1.10.2359475
    shared library libEGL.so -> /usr/lib/libEGL.so.1.10.2359475
    shared library libpvr2d.so -> /usr/lib/libpvr2d.so.1.10.2359475
    shared library libpvrPVR2D_BLITWSEGL.so -> /usr/lib/libpvrPVR2D_BLITWSEGL.so.1.10.2359475
    shared library libpvrPVR2D_FLIPWSEGL.so -> /usr/lib/libpvrPVR2D_FLIPWSEGL.so.1.10.2359475
    shared library libpvrPVR2D_FRONTWSEGL.so -> /usr/lib/libpvrPVR2D_FRONTWSEGL.so.1.10.2359475
    shared library libpvrPVR2D_LINUXFBWSEGL.so -> /usr/lib/libpvrPVR2D_LINUXFBWSEGL.so.1.10.2359475
    shared library libpvrEWS_WSEGL.so -> /usr/lib/libpvrEWS_WSEGL.so.1.10.2359475
    shared library libpvrEWS_REMWSEGL.so -> /usr/lib/libpvrEWS_REMWSEGL.so.1.10.2359475
    shared library libsrv_um.so -> /usr/lib/libsrv_um.so.1.10.2359475
    shared library libsrv_init.so -> /usr/lib/libsrv_init.so.1.10.2359475
    shared library libPVRScopeServices.so -> /usr/lib/libPVRScopeServices.so.1.10.2359475
    shared library libews.so -> /usr/lib/libews.so.1.10.2359475
    binary pvrsrvctl -> /usr/local/bin/pvrsrvctl
    binary sgx_init_test -> /usr/local/bin/sgx_init_test
    binary ews_server -> /usr/local/bin/ews_server
    binary ews_server_es2 -> /usr/local/bin/ews_server_es2
    binary services_test -> /usr/local/bin/services_test
    binary sgx_blit_test -> /usr/local/bin/sgx_blit_test
    binary sgx_clipblit_test -> /usr/local/bin/sgx_clipblit_test
    binary sgx_flip_test -> /usr/local/bin/sgx_flip_test
    binary sgx_render_flip_test -> /usr/local/bin/sgx_render_flip_test
    binary pvr2d_test -> /usr/local/bin/pvr2d_test
    binary gles1test1 -> /usr/local/bin/gles1test1
    binary gles1_texture_stream -> /usr/local/bin/gles1_texture_stream
    binary gles2test1 -> /usr/local/bin/gles2test1
    shader glsltest1_vertshader.txt -> /usr/local/bin/glsltest1_vertshader.txt
    shader glsltest1_fragshaderA.txt -> /usr/local/bin/glsltest1_fragshaderA.txt
    shader glsltest1_fragshaderB.txt -> /usr/local/bin/glsltest1_fragshaderB.txt
    binary gles2_texture_stream -> /usr/local/bin/gles2_texture_stream
    binary eglinfo -> /usr/local/bin/eglinfo
    binary ews_test_gles1 -> /usr/local/bin/ews_test_gles1
    binary ews_test_gles2 -> /usr/local/bin/ews_test_gles2
    shader ews_test_gles2_main.vert -> /usr/local/bin/ews_test_gles2_main.vert
    shader ews_test_gles2_main.frag -> /usr/local/bin/ews_test_gles2_main.frag
    shader ews_test_gles2_pp.vert -> /usr/local/bin/ews_test_gles2_pp.vert
    shader ews_test_gles2_pp.frag -> /usr/local/bin/ews_test_gles2_pp.frag
    binary ews_test_swrender -> /usr/local/bin/ews_test_swrender

    Installation complete!
    You may now reboot your target.

    Disabling lock debugging due to kernel taint
    +++++++++++++ PVRCore_Init 1031 +++++++++++++
    +++++++++++++ PVRCore_Init 1046 +++++++++++++
    PVR: PVRCore_Init
    +++++++++++++ PVRCore_Init 1051 +++++++++++++
    +++++++++++++ PVRCore_Init 1057 +++++++++++++
    +++++++++++++ PVRCore_Init 1064 +++++++++++++
    +++++++++++++ PVRCore_Init 1071 +++++++++++++
    +++++++++++++ PVRCore_Init 1074 +++++++++++++
    +++++++++++++ PVRCore_Init 1083 +++++++++++++
    +++++++++++++ PVRCore_Init 1097 +++++++++++++
    +++++++++++++ PVRCore_Init 1112 +++++++++++++
    +++++++++++++ PVRCore_Init 1151 +++++++++++++
    PVR: PVRCore_Init: major device 251
    +++++++++++++ PVRCore_Init 1176 +++++++++++++
    +++++++++++++ PVRCore_Init 1194 +++++++++++++
    +++++++++++++ PVRSRVOpen 839 +++++++++++++
    +++++++++++++ PVRSRVOpen 853 +++++++++++++
    PVR:(Error): OpenServices: Cannot open device driver /dev/pvrsrvkm. [79, /pvr_bridge_u.c]
    PVR:(Error): PVRSRVInitSrvConnect: PVRSRVConnect failed [2413, /bridged_pvr_glue.c]
    PVR:(Error): SrvInit: PVRSRVInitSrvConnect failed (4) [37, /srvinit.c]
    /usr/local/bin/pvrsrvctl: SrvInit failed (already initialized?) (err=4)
    root@am335x-evm:~# ls -l /dev/pvrsrvkm                                                                                                        
    crw-rw-rw-    1 root     root      251,   0 Jun 26 02:24 /dev/pvrsrvkm

  • 你好,请问你问题解决了吗?我也碰到类似的问题,提示找不到文件linux/platform_data/sgx-omap.h 硬件用的AM3358,软件为SDK6.0,Graphics SDK版本为5_01_01_02