你好:
采用TMS320C6713B 芯片,外接16位FLASH ,在线运行正常,但是无法boot,DSP外部 配置管脚按手册要求进行配置,M0下拉4.7K电阻到地,M1上拉4.7K电阻到3.3V,发现不能boot后,测试M0管脚电压为0.5V,M1管脚电压为2.9V,查手册该电平值也在电平范围内。请大侠们指点。
另外在调试程序时,配置片内时钟出错,导致内部时钟运行在800M,不知是否与这有关?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
采用TMS320C6713B 芯片,外接16位FLASH ,在线运行正常,但是无法boot,DSP外部 配置管脚按手册要求进行配置,M0下拉4.7K电阻到地,M1上拉4.7K电阻到3.3V,发现不能boot后,测试M0管脚电压为0.5V,M1管脚电压为2.9V,查手册该电平值也在电平范围内。请大侠们指点。
另外在调试程序时,配置片内时钟出错,导致内部时钟运行在800M,不知是否与这有关?
数据手册43页上的注释对上下拉电阻有要求, 之前的4.7ohm有问题.
use external pullup or pulldown resistors no greater than 4.4 kΩ and 2.0 kΩ , respectively.
boot后, 你量一下EMIF上是否有数据被DSP读取?