This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP138 路径问题



**** Build of configuration Debug for project arm_ceshi ****

D:\ti\ccsv5\utils\bin\gmake -k all
'Building file: ../main.c'
'Invoking: ARM Compiler'
"D:/ti/ccsv5/tools/compiler/tms470_4.9.5/bin/cl470" -mv5e --code_state=32 --abi=eabi -me -g --include_path="D:/ti/ccsv5/tools/compiler/tms470_4.9.5/include" --include_path="C:/Users/zhang/workspace_v5_2/arm_ceshi/inc" --include_path="C:/Users/zhang/workspace_v5_2/arm_ceshi/gel" --define=omapl138 --define=omapl137 --diag_warning=225 --display_error_number --preproc_with_compile --preproc_dependency="main.pp" "../main.c"
'Finished building: ../main.c'
' '
'Building target: arm_ceshi.out'
'Invoking: ARM Linker'
"D:/ti/ccsv5/tools/compiler/tms470_4.9.5/bin/cl470" -mv5e --code_state=32 --abi=eabi -me -g --define=omapl138 --define=omapl137 --diag_warning=225 --display_error_number -z --stack_size=0x800 -m"arm_ceshi.map" --heap_size=0x800 -i"D:/ti/ccsv5/tools/compiler/tms470_4.9.5/lib" -i"D:/ti/ccsv5/tools/compiler/tms470_4.9.5/include" --reread_libs --warn_sections --display_error_number --rom_model -o "arm_ceshi.out" "./main.obj" -l"D:\ti\ccsv5\tools\compiler\tms470_4.9.5\lib\libc.a" -l"C:\Users\zhang\workspace_v5_2\arm_ceshi\lib\evmomapl138_bsl.lib" -l"C:\Users\zhang\workspace_v5_2\arm_ceshi\lib\evmomapl138_csl.lib" "../OMAPL138.cmd" "../lib/evmomapl138_bsl.lib" "../lib/evmomapl138_csl.lib"
<Linking>

undefined first referenced
symbol in file
--------- ----------------
EVMOMAPL138_pinmuxConfig ./main.obj
GPIO_setDir ./main.obj
GPIO_setOutput ./main.obj
I2C_init ./main.obj
USTIMER_delay ./main.obj
USTIMER_init ./main.obj

error #10234-D: unresolved symbols remain

error #10010: errors encountered during linking; "arm_ceshi.out" not built
>> Compilation failure
gmake: *** [arm_ceshi.out] Error 1
gmake: Target `all' not remade because of errors.

**** Build Finished ****