手里有个VOIP的电话机项目,需要+点对点(D1分辨率)视频,准备考虑使用OMAP3525,请问TI专家~
1、用OMAP3525是否合适?
2、官网上推荐DM3725替代OMAP3525,是否OMAP系列要停产了?
3、语音、图像处理准备用官方的库;但由于对DSP不太了解,可能遇见的几个关键问题,如噪声抑制、回声抵消、包括和SLIC芯片驱动等,有哪些第三方资源可有偿获取?
谢谢~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. 需要跑什么操作系统?要不要显示界面?
2. 编解码的格式是什么,需要什么编码格式?性能要求我理解为同编同解D1分辨率即可,对吗
3. 显示屏幕的分辨率帧率和接口要求,是否需要双方画面同时显示/画中画
4. 我们有一些DSP上跑的音频库,如AER等。http://www.ti.com/tool/TELECOMLIB?keyMatch=volib&tisearch=Search-EN
OMAP3和DM3725都是用内置DSP来做编解码的,性能够,但是会消耗DSP的性能。
PIP的支持我不是很确定。其他的要求都是能够满足的。
请问你这边是已经有了OMAP3525或者DM37x的开发经验吗?还是全新开始。