This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

问题:AM3352的SPI norflash能接多大的flash?



大家好:

   我看到datasheet关于spi flash启动有这样描述:

  26.1.7.6.1 Features
      • Supports 12-MHz clock (50% duty cycle).
      • Supports only SPI Mode 3 (clock polarity = 1, clock phase = 1).
      • Supports only 24-bit addressable EEPROMs.
      • Supports only 4-pin SPI mode (CS, CLK, Serial Input, Serial Output).
      • The boot devices must be connected to chip select 0 and must support the read command (03h).
      • The boot image is copied into internal memory and then executed.

这个说明spi只能接16M的norflash吗?目前我们项目想用32Mnorflash不知是否可行?谢谢!