This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x can 收发问题



1、参考 C:\ti\AM335X_StarterWare_02_00_01_01\examples\evmAM335x\dcanTxRx工程配置。

2、设置波特率250K。

3、测试通过CAN TX,RX引脚功能配置正确。

4、CAN发送数据,在收发器CAN_H,CAN_L用示波器,CAN协议解析数据,波特率设置为250K,测出正确数据。但是没有应答场信号。

5、CAN 设置为Loopback mode,发送,接收数据正确,在中断中能读取到接收数据。

6、CAN 设置为Silent mode,发送数据不正常,无中断信号。

7、CAN 设置为 Loopback mode combined with silent mode,发送,接收数据正常,中断中能获取收到数据。

这样情况是接收端配置问题吗? 要如何解决无应答场问题,谢谢!