This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6670 的SRIO低温测试问题



我们公司的板卡上有两个DSP,现在做低温测试,温度在-30C。

两个DSP均为tms320c6670,两个DSP均与FPGA通过SRIO互联。FPGA为Altera ArriaGx

SRIO模式为2.5Gbps,4x通道,srio输入时钟250MHz,DSP主频为983MHz。

问题描述:低温测试反复上电启动时,其中一个DSP容易出现SRIO初始化失败的故障,通过仿真器查看err_stat寄存器的portOKBit,出问题的时候总是

为低。

目前做过的测试:digitalloopback和serdesloopback,均为DSP内部环回,此时FPGA不工作。

digital环回反复上电测试初始化200余次均无故障,serdesloopback问题就很明显,概率和直通时的故障概率差不多。

我们的srio serdes基本配置如下:

PLLConfig:0x00000051

TxConfig:0x001807a5

RxConfig:0x004404a5

四个lane的Tx/Rx配置一样

现在想问两种内部环回测试结果不一样说明什么?serdes环回测试不稳定的原因如何分析?如何解决?

而且我们的系统原先都工作在3.125G,后来常温下初始化都经常出问题所以降到了2.5G才解决。现在低温2.5G的速率仍然有问题,该怎么分析?