你好:
请问am3358的LCD接口支持MCU或SPI的类型吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个问题的什么意思……
AM335x的LCD接口是RGB的,RGB888或者RGB565的。
如果你是想用AM335x和MCU对接,通信方式是SPI的话,AM335x上面是有SPI接口的,可以做主也可以做从,只要MCU那段有SPI就可以。
你后面的几张图像是使用SPI接口,前面的那些又像是一个显示类型的接口。建议你先搞清楚,你原来的这些接口都是用来做什么的,是接LCD屏幕的?还是MCU和其他device之间进行通信的?
你好:
上面的这些接口都是LCD屏的接口,我想问的是AM335X是只能接RGB接口的LCD屏还是说上面列出来的这几种LCD屏的接口有些也是能接的?