Hi, Ti的技术支持
请帮忙确认一下AM335x处理器的Timer7工作是否正常,分下面二种情况进行测试:
1. 在cpsw驱动中,将定时器改成Timer6和Timer7的组合,测试网络功能是否正常,原来用的定时器是Timer5和Timer6
2. 将Timer7设置成time或才compare模式,看看那个Timer7的管脚是否有输出
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Ti的技术支持
请帮忙确认一下AM335x处理器的Timer7工作是否正常,分下面二种情况进行测试:
1. 在cpsw驱动中,将定时器改成Timer6和Timer7的组合,测试网络功能是否正常,原来用的定时器是Timer5和Timer6
2. 将Timer7设置成time或才compare模式,看看那个Timer7的管脚是否有输出
谢谢!
你好,我用的是AM3352芯片,那为什么只能用timer5和timer6这样的组合最好呢?
我测试过,如果换成timer4和timer5的组合,网络驱动还可以,就是时延稍未大一点。
如果换成timer6和timer7就几乎不能工作了,时延超过1000ms,这是为什么?
我从网上看到的有新的驱动,但适合高版本的Linux内核,我现在用的Linux内核只有3.1.0。
现在的关键是Timer7管脚能输出也没有问题,我可以改版,假如cpsw能够直接使用Timer4和Timer7那是最佳的,但实际不能够用,我测试过。
新的版本的驱动,也有用到定时器,只是没有使用Timer4~到Timer7之间的通用定时器,而且但有用到系统的定时器,不知道那个定时器是不是和原来的功能一样就不清楚了。