This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6455 TCP2 译码算法



想问下TCP2中两种译码算法的使用相关:

我们目前的测试显示:Max-Log-Map算法要比Max*好很多。系统使用的是16QAM的Turbo编码,二者的输入都是LLR的软解调数据,里面包含了信噪比估计的噪声功率。但是理论上Max*要比Max-Log-Map好。想问下MAX*的LLR需要乘以一个因子吗?如果乘以。这个因子具体式子怎么表示?

附:理想信噪比估计,16QAM,Turbo码的系统,测试数据导入10^7,EbN0=6.4dB,Max-Log-Map误比特率为1.5e-04,Max*是2.5e-02。