This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am335x_spi_partitions在什么地方!



sdk 8.0下面的分区文件在什么地方啊,一直都找不到!
/* SPI 0/1 Platform Data */
/* SPI flash information */
static struct mtd_partition am335x_spi_partitions[] = {
    /* All the partition sizes are listed in terms of erase size */
    {
        .name       = "SPL",
        .offset     = 0,            /* Offset = 0x0 */
        .size       = SZ_128K,
    },
    {
        .name       = "U-Boot",
        .offset     = MTDPART_OFS_APPEND,   /* Offset = 0x20000 */
        .size       = 2 * SZ_128K,
    },
    {
        .name       = "U-Boot Env",
        .offset     = MTDPART_OFS_APPEND,   /* Offset = 0x60000 */
        .size       = 2 * SZ_4K,
    },
    {
        .name       = "Kernel",
        .offset     = MTDPART_OFS_APPEND,   /* Offset = 0x62000 */
        .size       = 28 * SZ_128K,
    },
    {
        .name       = "File System",
        .offset     = MTDPART_OFS_APPEND,   /* Offset = 0x3E2000 */
        .size       = MTDPART_SIZ_FULL,     /* size ~= 4.1 MiB */
    }
};
  • 在SDK06.00(kernel为3.2及之前)及以前的版本,通常你会在Linux/arch/arm/mach-omap2/board-am335xevm.c中找到;

    而在SDK07.00(kernel为3.12)和SDK08.00(kernel 为3.14) ,由于linux源码中没有对应的板级文件,板级配置通过devicetree进行。

    所以你可以参考am335x-evm.dts里面的nand flash的分区,添加SPI的分区。

  • 非常感谢,我看到board-am335xevm.c中,有下面这段:

    /* MTD partition table */
    /* All SPL-* partitions are sized to minimal length
    * which can be independently programmable. For
    * NAND flash this is equal to size of erase-block */

    是不是下面的nand分区不用改就可以用作spi分区啊,刚接触TI,很多不懂,如果不是的,能否提供一下spi分区的例子啊,跪求!


    #address-cells = <1>;
    #size-cells = <1>;
    partition@0 {
    label = "NAND.SPL";
    reg = <0x00000000 0x000020000>;
    };
    partition@1 {
    label = "NAND.SPL.backup1";
    reg = <0x00020000 0x00020000>;
    };
    partition@2 {
    label = "NAND.SPL.backup2";
    reg = <0x00040000 0x00020000>;
    };
    partition@3 {
    label = "NAND.SPL.backup3";
    reg = <0x00060000 0x00020000>;
    };
    partition@4 {
    label = "NAND.u-boot-spl-os";
    reg = <0x00080000 0x00040000>;
    };
    partition@5 {
    label = "NAND.u-boot";
    reg = <0x000C0000 0x00100000>;
    };
    partition@6 {
    label = "NAND.u-boot-env";
    reg = <0x001C0000 0x00020000>;
    };
    partition@7 {
    label = "NAND.u-boot-env.backup1";
    reg = <0x001E0000 0x00020000>;
    };
    partition@8 {
    label = "NAND.kernel";
    reg = <0x00200000 0x00800000>;
    };
    partition@9 {
    label = "NAND.file-system";
    reg = <0x00A00000 0x0F600000>;
    };