This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368+IPNC4.1.0 在5M分辨率下支持双码流吗?



请问下,DM368+IPNC4.1.0 在5M分辨率下支持双码流吗?
现在我的情况是这样子的:
1. DM368+IPNC4.1.0, 使用500W sensor - MT9P031,如果只开启主码流为 5M@10fps, 可以正常编码输出,主码流低于3M及以下时可以正常输出双码流
2. 在主码流为5M的基础上,修改IPNC代码增加一路子码流,此时主码流图像就会出现不连贯,而子码流则比较正常
3. 在第二种情形下修改主码流的 I 帧间隔为1,则可以使主码流图像连贯,但会出现比较多的马赛克。在 I 帧间隔大于1时,修改主码流或者子码流的帧率或码率都不会改善主码流不连贯的问题
所以我的问题是,DM368 在主码流为5M的情况下支持同时输出子码流吗,如果支持的话在这种情况下需要修改哪些设置呢?

谢谢!