This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM3730,DM3725,AM3715,AM3703功耗比较及选型



问题背景:做一个cmos图像采集的项目,但并不输出视频流,仅仅是对每帧图像进行一些特定的算法运算,提取出每幅图像的位置信息并输出。DM3730的camera 的接口很方便,同时有POP封装,满足小尺寸的需求,但唯一的问题是现在不确定算法量,对功耗不好确定,看到手册里800Mhz工作时给出的含pop memory的功耗是1.42W,这个值高于我们的预期。

问题1:DM3730内部的SGX模块不需要的话,在软件里不调用能使它仅仅是待机模式么,这样功耗会降低多少,还有大部分接口模块也不需要,功耗会有多少降低的空间啊(问题可能都比较简单或者理解有错误,请见谅)

问题2:AM37x系列手册里提供的800Mhz工作时给出的含pop memory的功耗仍是1.42W,这个值为什么与DM37x的一致?

问题3:DM3730DM3725AM3715AM3703是pin-to-pin兼容,构架看上去也基本相同,这样是否可以做到我先用DM3730开发,硬件、软件都不需要有所改动就可以换成DM3725AM3715AM3703的片子(目前算法仅在matlab完成,优先考虑在DM3730的DSP中实现,如果功耗实测过大,ARM跑算法运算速率又够用,希望换成无DSP核的AM37X),不知这样的步骤是否可行

问题4:POP封装支持的memory是否只有美光,有没有官方推荐的型号