在DM385下面原本支持的有tvp5158,tvp7002,sii9022,sii9135。
但是我现在板子上使用的处理芯片是sii1161,不知道我应该如何添加sii1161的驱动支持呢?
在ipnc_rdk下。
希望得到帮助,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这颗芯片是什么输出接口呢?是否可以配置成类似tvp7002/sil9 目前RDK原生支持的接口,那样就可以直接沿用原来的采集部分的配置了。
另一个部分就是对于Sil1161的配置,通常这类芯片可以通过I2C来导入寄存器值的,可以去找厂家获得。
sii1161的接口和sii9的差异比较大,不能照搬sii9的来用。
寄存器属性已经找到,但似乎现在只能重新写一个驱动。
是否在其他软件包里面会包含了sii1161的驱动了呢?
目前DM81xx/DM38x相关的SDK都没有包含Sii1161的驱动,不过你可以参考下面的链接:
http://processors.wiki.ti.com/index.php/DM81xx_AM38xx_Adding_External_Decoders_to_V4L2_Capture_Driver