This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问DM385 的./bin/sys_pri.out --L3-bw-reg-set, HDVICP0和ISS 设置Bandwidth 上限是多少?



您好!

我打算使用./bin/sys_pri.out --L3-bw-reg-set 调节 HDVICP0和ISS的参数。

但是不清楚"L3-Bandwidth", "L3-Watermark-cycles"范围是多少?

我可以这么修改吗?

./bin/sys_pri.out --L3-bw-reg-set HDVICP0 3 3 900 2500&
./bin/sys_pri.out --L3-bw-reg-set ISS 0 0 400 2500&