This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 IPNC 4.0 错误



以下是启动时的打印输出

## Booting kernel from Legacy Image at 80700000 ...
Image Name: Linux-2.6.37_IPNC_DM365_4.0.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3842496 Bytes = 3.7 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK

Starting kernel ...

[ 0.000000] Linux version 2.6.37_IPNC_DM365_4.0.0 (root@ubuntu) (gcc version 4.3.3 (GCC) ) #1 PREEMPT Sun Apr 12 22:06:44 PDT 2015
[ 0.000000] CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
[ 0.000000] CPU: VIVT data cache, VIVT instruction cache
[ 0.000000] Machine: DaVinci DM36x IPNC
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] DaVinci dm36x_rev1.2 variant 0x8
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 15240
[ 0.000000] Kernel command line: mem=60M console=ttyS0,115200n8 root=/dev/nfs nfsroot=192.168.1.47:/home/ipnc/dm368_dvsdk/Source/ipnc_rdk/target/filesys rw ip=dhcp video=davincifb:vid0=OFF:vid1=OFF:osd0=720x576x16,2025K dm365_imp.oper_mode=0 davinci_capture.device_type=2 video=dm36x:output=pal
[ 0.000000] PID hash table entries: 256 (order: -2, 1024 bytes)
[ 0.000000] Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.000000] Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Memory: 60MB = 60MB total
[ 0.000000] Memory: 56964k/56964k available, 4476k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] DMA : 0xff000000 - 0xffe00000 ( 14 MB)
[ 0.000000] vmalloc : 0xc4000000 - 0xfea00000 ( 938 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xc3c00000 ( 60 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .init : 0xc0008000 - 0xc002a000 ( 136 kB)
[ 0.000000] .text : 0xc002a000 - 0xc038b000 (3460 kB)
[ 0.000000] .data : 0xc038c000 - 0xc03b21c0 ( 153 kB)
[ 0.000000] SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptable hierarchical RCU implementation.
[ 0.000000] RCU-based detection of stalled CPUs is disabled.
[ 0.000000] Verbose stalled-CPUs detection is disabled.
[ 0.000000] NR_IRQS:245
[ 0.000000] Console: colour dummy device 80x30
[ 0.000408] Calibrating delay loop... 147.86 BogoMIPS (lpj=739328)
[ 0.220097] pid_max: default: 32768 minimum: 301
[ 0.220523] Mount-cache hash table entries: 512
[ 0.221600] CPU: Testing write buffer coherency: ok
[ 0.227641] DaVinci: 8 gpio irqs
[ 0.228475] NET: Registered protocol family 16
[ 0.248427] EVM: (null) video input
[ 0.354925] bio: create slab <bio-0> at 0
[ 0.361530] SCSI subsystem initialized
[ 0.366634] usbcore: registered new interface driver usbfs
[ 0.368409] usbcore: registered new interface driver hub
[ 0.369635] usbcore: registered new device driver usb
[ 0.374298] vpss vpss: dm365_vpss vpss probed
[ 0.374385] vpss vpss: dm365_vpss vpss probe success
[ 0.376876] Advanced Linux Sound Architecture Driver Version 1.0.23.
[ 0.379524] Switching to clocksource timer0_1
[ 0.380130] Switched to NOHz mode on CPU #0
[ 0.464277] NET: Registered protocol family 2
[ 0.464688] IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.465768] TCP established hash table entries: 2048 (order: 2, 16384 bytes)
[ 0.465972] TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.466101] TCP: Hash tables configured (established 2048 bind 2048)
[ 0.466148] TCP reno registered
[ 0.466207] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.466297] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.466990] NET: Registered protocol family 1
[ 0.468346] RPC: Registered udp transport module.
[ 0.468408] RPC: Registered tcp transport module.
[ 0.468447] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.568620] Installing knfsd (copyright (C) 1996 okir@monad.swb.de).
[ 0.570028] JFFS2 version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.
[ 0.575108] msgmni has been set to 111
[ 0.580667] io scheduler noop registered (default)
[ 0.582712] CSL: Module install successful, device major num = 254
[ 0.582777] CSL: Module version 0.10.00, built on Apr 12 2015 21:58:32
[ 0.582847] I2C: Module install successful, device major num = 253
[ 0.582902] DMA: Module install successful, device major num = 252
[ 0.582942] DRV: Module install successful
[ 0.582977] DRV: Module built on Apr 12 2015 21:58:34
[ 0.583014] DRV: EDMACC.QUEPRI = 00002777
[ 0.583046] DRV: SYSTEM.MSTPRI0 = 00440011
[ 0.583078] DRV: SYSTEM.MSTPRI1 = 00000444
[ 0.583109] DRV: ISP.BCR = 00000002
[ 0.583141] DRV: SYSTEM.MISC = 00000399
[ 0.583174] EDMAK module: built on Apr 12 2015 at 21:58:15
[ 0.583215] Reference Linux version 2.6.37
[ 0.583252] File /home/ipnc/dm368_dvsdk/Source/dvsdk_ipnctools/linuxutils_2_26_02_05/packages/ti/sdo/linuxutils/edma/src/module/edmak.c
[ 0.585185] IRQK module: built on Apr 10 2015 at 01:10:41
[ 0.585254] Reference Linux version 2.6.37
[ 0.585291] File /home/ipnc/dm368_dvsdk/Source/dvsdk_ipnctools/linuxutils_2_26_02_05/packages/ti/sdo/linuxutils/irq/src/module/irqk.c
[ 0.587286] irqk initialized
[ 0.587382] CMEMK module: built on Apr 12 2015 at 21:58:13
[ 0.587434] Reference Linux version 2.6.37
[ 0.587472] File /home/ipnc/dm368_dvsdk/Source/dvsdk_ipnctools/linuxutils_2_26_02_05/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c
[ 0.589362] no physical memory specified, continuing with no memory allocation capability...
[ 0.589504] cmemk initialized
[ 0.589561] Serial: 8250/16550 driver, 2 ports, IRQ sharing disabled
[ 0.614962] serial8250.0: ttyS0 at MMIO 0x1c20000 (irq = 40) is a 16550A
[ 1.116752] console [ttyS0] enabled
[ 1.142939] serial8250.0: ttyS1 at MMIO 0x1d06000 (irq = 41) is a 16550A
[ 1.154367] brd: module loaded
[ 1.169220] NAND device: Manufacturer ID: 0xec, Chip ID: 0xf1 (Samsung )
[ 1.178129] Bad block table not found for chip 0
[ 1.184606] Bad block table not found for chip 0
[ 1.189263] Scanning device for bad blocks
[ 1.284419] Creating 7 MTD partitions on "davinci_nand.0":
[ 1.290133] 0x000000000000-0x000000300000 : "bootloader"
[ 1.300920] 0x000000300000-0x000000500000 : "params"
[ 1.311485] 0x000000500000-0x000000900000 : "kernel"
[ 1.322250] 0x000000900000-0x000003100000 : "filesystem1"
[ 1.333558] 0x000003100000-0x000003300000 : "data1"
[ 1.344323] 0x000003300000-0x000005b00000 : "filesystem2"
[ 1.355898] 0x000005b00000-0x000008000000 : "data2"
[ 1.366829] davinci_nand davinci_nand.0: controller rev. 2.3
[ 1.429749] davinci_mdio davinci_mdio.0: davinci mdio revision 1.4
[ 1.435988] davinci_mdio davinci_mdio.0: detected phy mask fffffffd
[ 1.444209] davinci_mdio.0: probed
[ 1.447679] davinci_mdio davinci_mdio.0: phy[1]: device 0:01, driver unknown
[ 1.455861] i2c /dev entries driver
[ 1.462318] Linux media interface: v0.10
[ 1.467216] Linux video capture interface: v2.00
[ 1.474936] vpbe-osd vpbe-osd: OSD sub device probe success
[ 1.481940] vpbe-venc vpbe-venc: VENC sub device probe success
[ 1.489122] vpbe-v4l2 vpbe-v4l2: vpbe v4l2 device registered
[ 1.495324] Setting default output to Composite
[ 1.500126] Setting default mode to ntsc
[ 1.504224] vpbe-v4l2 vpbe-v4l2: Trying to register VPBE display device.
[ 1.511100] vpbe-v4l2 vpbe-v4l2: layer=c3564200,layer->video_dev=c35642e8
[ 1.518990] vpbe-v4l2 vpbe-v4l2: Trying to register VPBE display device.
[ 1.526059] vpbe-v4l2 vpbe-v4l2: layer=c3450000,layer->video_dev=c34500e8
[ 1.535345] watchdog watchdog: heartbeat 60 sec
[ 1.547206] Error: Driver 'davinci-mcbsp' is already registered, aborting...
[ 1.558225] asoc: cq93vc-hifi <-> davinci-vcif mapping ok
[ 1.568503] ALSA device list:
[ 1.571921] #0: DaVinci DM365 EVM
[ 1.577247] TCP cubic registered
[ 1.580963] NET: Registered protocol family 17
[ 1.597734] net eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, id=181b8a0)
[ 1.620111] Sending DHCP requests .
[ 3.590039] PHY: 0:01 - Link is Up - 100/Full
[ 4.359697] ., OK
[ 4.869756] IP-Config: Got DHCP answer from 0.0.0.0, my address is 192.168.1.118
[ 4.877983] IP-Config: Complete:
[ 4.881219] device=eth0, addr=192.168.1.118, mask=255.255.255.0, gw=192.168.1.1,
[ 4.889059] host=192.168.1.118, domain=, nis-domain=(none),
[ 4.895199] bootserver=0.0.0.0, rootserver=192.168.1.47, rootpath=
[ 5.042215] VFS: Mounted root (nfs filesystem) on device 0:13.
[ 5.048085] VFS: mounted rootfs
[ 5.051642] Freeing init memory: 136K
INIT: version 2.86 booting
Starting mounting local filesystems: mount Creat queue id:0
queue id:0
FileMngThread created
Creat queue id:32769
queue id:32769
AlramThread created
Share memory init success
IPNC_DM365_4.0.0 (root@ubuntu) (gcc version 4.3.3 (GCC) ) #1 PREEMPT Sun Apr 1
Creat queue id:65538
queue id:65538
queue id:32769
queue id:65538
Creat queue id:98307
queue id:98307
net_search_gateway:eth0, 1A8C0, 0, 1

CPU is DM365

*****************************************************************

IPNC BUILD VERSION: DM365 IPNC RDK V4.00.00.08

*****************************************************************

./av_server.out DM365 NTSC APPRO2A AEWB 720P H264 4000000 VBR AUTO MENUOFF &
Check_device_version : DEVICE VER = 1 !!

在该位置会等待大约5分钟左右


[ 14.492850] nfs: server 192.168.1.47 not responding, still trying
[ 14.499274] nfs: server 192.168.1.47 not responding, still trying
[ 14.505641] nfs: server 192.168.1.47 not responding, still trying
[ 16.972812] nfs: server 192.168.1.47 not responding, still trying
[ 22.892826] nfs: server 192.168.1.47 not responding, still trying
[ 83.305118] nfs: RPC call returned error 22
[ 83.404322] nfs: server 192.168.1.47 OK
[ 83.409083] nfs: server 192.168.1.47 OK
[ 83.413764] nfs: server 192.168.1.47 OK
[ 83.417875] nfs: server 192.168.1.47 OK
mount: mounting /dev/root on / failed: No such file or directory
failed (1: ).
ApproDrvInit: 7
Creat queue id:131076
queue id:131076
Starting internet superserver: inetd
DM365MM Init Successful
AVSERVER UI: Initializing.
.

CLK Hz,
ARM Hz = 297000000
DDR Hz = 243000000
VPSS Hz = 243000000
IMCOP Hz = 243000000

[ 85.551118] CMEMK Error: ioctl: no heap available in block 0
CMEM Error: allocHeap: ioctl CMEM_IOCALLOCHEAP failed: -1
[ 86.113727] CMEMK Error: Failed to find a pool which fits 28672
CMEM Error: getP[ 86.135877] CMEMK Error: get_phys: Unable to find phys addr for 0x00000000
ool: Failed to get a pool fitting a size 28672
[ 86.151912] CMEMK Error: get_phys: get_user_pages() failed: -14
[ 86.164612] CMEMK Error: GETPHYS: Failed to convert virtual 0x0 to physical.
CMEM Error: getPhys: Failed to g[ 86.174086] CMEMK Error: get_phys: Unable to find phys addr for 0x00000000
et physical address of 0
[ 86.192232] CMEMK Error: get_phys: get_user_pages() failed: -14
[ 86.203777] CMEMK Error: FREE: Failed to convert virtual 0x0 to physical
CMEM Error: free: failed to free 0
ERROR (alg.c|ALG_sysInit|82): VICP Protocol regn failed
ERROR (avServerApi.c|AVSERVER_init|580): ALG_sysInit()
ERROR (avServerUi.c|UI_start|58): AVSERVER_init()
insmod: can't read '/opt/ipnc/modules/deflate.ko': No such file or directory
insmod: can't read '/opt/ipnc/modules/des_generic.ko': No such file or directory
insmod: can't read '/opt/ipnc/modules/md5.ko': No such file or directory
ApproDrvInit: 8
ApproDrvInit: 9
ApproDrvInit: 6
queue id:131076
ApproDrvInit: 10
queue id:131076
ApproDrvInit: 2
queue id:131076
queue id:131076
queue id:131076
[ 87.769712] davinci_mmc davinci_mmc.0: Using DMA, 4-bit mode
[ 88.063541] Loading iSCSI transport class v2.0-870.
[ 88.645276] iscsi: registered transport (tcp)
[ 88.825583] musb-hdrc: version 6.0, peripheral, debug=0
[ 89.026241] musb-hdrc musb-hdrc: dma type: dma-cppi3
[ 89.046369] musb-hdrc musb-hdrc: USB Peripheral mode controller at fec64000 using DMA, IRQ 12
[ 89.293304] loop: module loaded
[ 89.421505] tun: Universal TUN/TAP device driver, 1.6
[ 89.427090] tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
[ 89.652651] console [netcon0] enabled
[ 89.656817] netconsole: network logging started
[ 89.823474] PPP generic driver version 2.4.2
[ 89.890939] PPP Deflate Compression module registered
mkdosfs 2.11 (12 Mar 2005)
unable to get drive geometry, using default 255/63/dev/ram0 has 255 heads and 63 sectors per track,
logical sector size is 512,
using 0xf8 media descriptor, with 8192 sectors;
file system has 2 12-bit FATs and 4 sectors per cluster.
FAT size is 6 sectors, and provides 2036 clusters.
Root directory contains 512 slots.
Volume ID is 000003da, no volume label.
queue id:0
TimeOut occure in boot_proc.
Program exit.
ApproDrvInit: 3
queue id:131076
INIT: Entering runlevel: 5
Starting telnet daemon.
Starting syslogd/klogd: done
getty: ioctl() TIOCSPGRP call failed
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|

Arago Project http://arago-project.org 192.168.1.118 console

Arago 2009.11 192.168.1.118 console

192.168.1.118 login: root
-sh: can't access tty; job control turned off
root@192:~#
root@192:~#

请问是什么原因造成停留5分钟,

看上去像是NFS有些问题,

但是等待之前明明有如下信息


[ 4.895199] bootserver=0.0.0.0, rootserver=192.168.1.47, rootpath=

[ 5.042215] VFS: Mounted root (nfs filesystem) on device 0:13.
[ 5.048085] VFS: mounted rootfs

说明NFS已经挂载完成了,

不解

还有一点,

启动时有

[ 1.580963] NET: Registered protocol family 17
[ 1.597734] net eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, id=181b8a0)
[ 1.620111] Sending DHCP requests .
[ 3.590039] PHY: 0:01 - Link is Up - 100/Full
[ 4.359697] ., OK
[ 4.869756] IP-Config: Got DHCP answer from 0.0.0.0, my address is 192.168.1.118
[ 4.877983] IP-Config: Complete:
[ 4.881219] device=eth0, addr=192.168.1.118, mask=255.255.255.0, gw=192.168.1.1,
[ 4.889059] host=192.168.1.118, domain=, nis-domain=(none),

那么我的机器应该是通过DHCP获得了IP:192.168.1.118

但是当我查看网口信息时却不是

root@192:/# ifconfig -a
eth0 Link encap:Ethernet HWaddr DE:AD:BE:AF:00:00
inet addr:192.168.1.168 Bcast:192.168.1.255 Mask:255.255.255.0
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:8307 errors:0 dropped:0 overruns:0 frame:0
TX packets:5749 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:10360006 (9.8 MiB) TX bytes:658392 (642.9 KiB)
Interrupt:52 Base address:0x7000

eth0:3 Link encap:Ethernet HWaddr DE:AD:BE:AF:00:00
inet addr:169.254.5.55 Bcast:169.254.255.255 Mask:255.255.0.0
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
Interrupt:52 Base address:0x7000

lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
UP LOOPBACK RUNNING MTU:16436 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

请问这个怎么解决,谢谢