1、自己设计的板子,6678 CVDD采用TPS56121+LM10011实现,参照6678手册要求,CVDD启动时为1.1V,可调范围设计成0.7~1.1V。但问题来了,在1G情况下DSP的8个核有时候能全部Boot成功,有时候某几个核会不能Boot起来,当降低频率到600多兆后,基本8个每次都能Boot起来。不知道是我买的DSP不行,还是我的板卡上电出现问题导致的,望大家给出点意见看看是什么原因引起的。
2、我用示波器测量EVM板的CVDD上电时序,发现EVM板上的CVDD刚启动时电压大约0.85V,复位释放后电压变成了0.999V,用CCS抓出它的VCNTL寄存器值为21~16位为101111,对照手册该值代表电压为1.001V,那么问题来了,为什么开发板的设计跟手册里描述的启动过程不一致呢??
3、我用示波器测量自己的板子CVDD上电顺序,发现刚启动时电压为1.11V,复位释放后电压变成了1.09V,查看VCNTL寄存器的21~16位的值为111110,该值设置是正确的,那么问题是为什么我的板子复位释放后电压还维持在1.1左右呢,为什么没有降到1V左右,是因为1.1太高导致我的DSP运行不稳定吗?