自己做的板子,使用DM8168芯片,软件平台是DVR-RDK3.0.
DDR3,2G,531MHz
采集芯片为sii9233A,双通道.
在采集双路1920x1200@60Hz情况下,开始运行demo后数分钟,采集程序崩溃.
提示信息如下:
897170:!!!SLAVE CORE [VPSS-M3] DOWN!!!
SystemLink_copySlaveCoreExceptionContext:146
mmap of [0xbe9e0000:36864]
mmap virt addresss:0x40169000
munmap of [0x40169000:36864]
SystemLink_copySlaveCoreExceptionContext:153
[m3vpss ] I2C: Arbitration lost !!!
[m3vpss ] !!!XDC RUNTIME ASSERT FAILED
[m3vpss ] xdc.runtime.Error @ ti.sysbios.gates.GateMutex: line 97:
[m3vpss ] assertion failure: A_badContext: bad calling context. See GateMutex API doc for details.
同样程序在另一块成品板子上,DDR3-667MHz,同样分辨率,可以稳定运行3小时以上.
求问TI大神,问题出在哪里.