This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不好意思,点发送的时候,内容突然就清空了。。。。。
是这样的,我用的是TMDXEVM6678LE开发板,想要用6678的SRIO接口与FPGA的SRIO接口实现互联,DSP端我用的是keystone-srio那个例程,可是只能测试通过SRIO_DIGITAL_LOOPBACK,其他测试模式SRIO_EXTERNAL_LINE_LOOPBACK,SRIO_EXTERNAL_FORWARD_BACK,SRIO_NO_LOOPBACK运行到检测port-ok寄存器时,总是过不去了,不知道该如何修改程序,还有就是我看了程序中的SRIO_EXTERNAL_LINE_LOOPBACK,SRIO_EXTERNAL_FORWARD_BACK这两种模式的描述,不是很明白他们之间的区别,望专家可以指点。谢谢!
您好,
SERDES_LOOPBACK的数据是在serdes处做回环,不会出DSP,所以如果你要将数据发出去给FPGA的话,肯定不能采用这种模式。目前我们提供一个BOC子板,可以将两块带AMC外接插槽的板卡链接在一起进行通信测试。如EVM板的SRIO外接到扩展口AMC,所以你也可以做一块FPGA板子将SRIO口做成标准的AMC外接口,然后插到我们的BOC板子就可以实现SRIO互通。
关于BOC板子参考:processors.wiki.ti.com/.../CI_Dual_EVM_Break_Out_Card