我用hex6x转化out文件时,运行"hex6x.exe hello.cmd"命令时提示fatal error: "hello.cmd", line 14: cannot open input file '/.out'”: no such file or directory(aborting).
其中:hello.out是我编译生成的out文件,hello.cmd是自己写的cmd文件。我已经将out文件,cmd文件以及hex6x放在了一个文件夹中。
hello.cmd文件如下:
hello.out //待转换的out 文件名
-a //二进制转换格式,这里用ASCII-Hex
-memwidth 8 //系统内存储器的每字节的位数,这里和Flash 一致,8 位;
-boot //生成引导程序表
-bootorg 0x02000400 //第二次载入程序的首地址
-bootsection .boot_load 0x02000000 //二次引导程序的首地址
ROMS
{
FLASH: org = 0x02000000, len = 0x1000000,romwidth = 8, files = {hello.hex}
}
请问问题出在哪?谢谢!!!