www.deyisupport.com/.../64648.aspx
续此贴,
fpga+7002把24bit或者30bit的数据转化为8bit的数据如何实现?
我理解是RGB的24bit数据按照YUV4:2:2格式转换成8bit的数据,再传给8168,不对吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
www.deyisupport.com/.../64648.aspx
续此贴,
fpga+7002把24bit或者30bit的数据转化为8bit的数据如何实现?
我理解是RGB的24bit数据按照YUV4:2:2格式转换成8bit的数据,再传给8168,不对吗?
Hi,
你的需求是用4颗TVP7002, 每颗TVP7002用RGB24bit接入,在FPGA中转换成8bit数据?
这个是可以实现的。 DM8168的8bit口,在嵌入同步的模式下实际就是用的BT656的SAV/EAV. 图像数据也是遵循着YUYV的顺序来的。是YUV422
BR,
Eason
我翻了下DM648的VIDEO PORT手册,最高80MHz,应该不能。
你看8bit的口,数据量上和16bit/24bit是一样的。1080p30的话在16bit/24bit下是74.25MHz那么在8bit下面就是148.5MHz
FPGA中,24bitRGB-》8bit中间大致需要如下转换:
RGB通过CSC色彩空间转换为YUV色彩空间;
YUV444下采样为16bitYUV422;
16bitYUV422转换为8bitYUV422。
FPGA IO口能多快?请咨询FPGA方面。。。