在AM3359 IDK开发板移植Linux系统中,使用系统的SDK工具包进行移植,在SD boot区中下载了MLO、u-boot.img和uImage 文件,SD卡 rootfs区中装载了文件系统filesystem,用SD卡启动,连接串口输入minicom指令电脑没反应。不知是文件有问题还是调试有问题?请问该连接开发板的哪个串口进行SD卡启动调试?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在AM3359 IDK开发板移植Linux系统中,使用系统的SDK工具包进行移植,在SD boot区中下载了MLO、u-boot.img和uImage 文件,SD卡 rootfs区中装载了文件系统filesystem,用SD卡启动,连接串口输入minicom指令电脑没反应。不知是文件有问题还是调试有问题?请问该连接开发板的哪个串口进行SD卡启动调试?
先确认你的串口输出是不是好的,验证方式可以设置为串口启动,查看是否会打印ccc出来。
确认串口没问题了后,再查MLO,MLO中配置了DDR这一步往往是最容易出问题的地方,确认这些配置成功了,MLO可以正常启动了后再往下走。
昨天才在英文 TI网站看到说am335x开发板的 linux SDK不支持IDK,原文pretty easy - there is no link because there is no Linux SDK supporting the IDK board. This has been discussed multiple times on this forum. Other boards kernel don't work because of different system hardware.。有给链接,
There is SYSBIOS examples available for IDK, please download from below link and try it.
但是对于链接中的文件不知道该怎么用才能完成移植