Part Number: AM625
问题描述:
官方的MCU_SDK只有R5核访问MMCSD控制器的例程,我现在需要通过MCU M4访问MMCSD.我选用empty作为基础项目在上面进行修改,通过example.syscfg进行MMCSD配置,但是并未找到相关选项,后来发现所有的M4核的example.syscfg都没有MMCSD选项,只有R5有。
如何在M4F下配置MMCSD呢?
M4F核项目的example.syscfg

R5核项目的example.syscfg

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM625
问题描述:
官方的MCU_SDK只有R5核访问MMCSD控制器的例程,我现在需要通过MCU M4访问MMCSD.我选用empty作为基础项目在上面进行修改,通过example.syscfg进行MMCSD配置,但是并未找到相关选项,后来发现所有的M4核的example.syscfg都没有MMCSD选项,只有R5有。
如何在M4F下配置MMCSD呢?
M4F核项目的example.syscfg

R5核项目的example.syscfg

您好
TI在下方链接答复过,建议避免从M4F核心使用MMCSD,可能会降低CPU性能, 而且TI也没有做过相关的验证。
看下方链接
SK-AM62: can MCU M4F access flash eMMC? - Processors forum - Processors - TI E2E support forums
您好
我尝试在在MCU M4F上布置MMCSD代码并进行调试。
1. 已经配置了RAT

2. 在操作寄存器时会卡死在那里,比如函数MMCSD_halSoftReset(...)下的代码
CSL_REG8_FINS(&pReg->SOFTWARE_RESET,
MMC_CTLCFG_SOFTWARE_RESET_SWRST_FOR_ALL,
CSL_MMC_CTLCFG_SOFTWARE_RESET_SWRST_FOR_ALL_VAL_RESET);
运行到这不会再往下运行了。
打印出SOFTWARE_RESET,的地址为0x8FA1002F,确认无误。
3. 我尝试在MMCSD代码中去读取其他控制器的某一个寄存器,如MCU_UART0-> _UART_EFR,可以成功运行并读取成功的。
地址为:0x84A00008