Hi,all
我在使用DM388通过CSI2接口连接IMX185,我现在已经按照185的手册修改为720P模式120fps,但是DM388无法正常工作,找到一些设置帧率的代码修改后还是不能正常运行,能帮忙指点一下需要修改思路。谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
1. 请提供具体的调试信息打印
2. 是否仍然使能了McTNF? 请注意这个滤波器是性能是1080p30的,所以灌720p120进去应该是超了的。
Hi,Eason
1.打印信息请见附件,分别是正常启动与设置为720P120fps的信息。我对比了一下,其他代码都不变,仅把stream.c中的STREAM_FEATURE_FRAMECTRL和STREAM_FEAUTRE_FRAMERATE1的参数值改为120帧。encLink_h264.c中EncLinkH264_algSetConfig中设置target和ref FrameRate的值限制在60000,即60帧,因此之前在dm36x上调试120帧时由于编码器的限制只能60,不知道dm388是否也有类似的限制,目前还没有阅读相关的文档。最后就是修改issdrv_imx185api.c中的配置了,按照185手册中720p120进行相关参数的修改。通过对比打印信息和调试发现似乎sensor没有数据输出。请问以上修改是否还有遗漏?

2.由于使用CSI-2接口,没有像并行接口那样的HD、VD可以测量实际的输出帧率,请问在CSI-2接口下怎样验证我是否成功把sensor设置为120fps模式呢?
谢谢。