This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

8127的tristreamfullfeature中,我将cameralink替换为capture+dei的后续基于cameralink的link的处理问题



大家好,我在8127上将sensor换成了模拟摄像头的输入,我首先在直通usecase上实验,可以成功捕获到数据,之后我修改link链接将数据送到A8核后保存了一帧图像,以证明我们的capturelink已经正常工作。

         接下来我希望在tristreamfullfeature这个默认usecase中将cameralink替换成capturelink+deilink,以实现网络端的UI界面查看图像,并实现8127自带的va功能(如人脸检测、trip zone等)。

         现在我遇到的问题是,在tristreamfullfeature这个默认usecase中,后面有许多link诸如isplink、valink、vstablink、vnflink、mctnflink等,这些link的Id是直接声明在参数cameraPrm中的,而相应的capturePrm中并未有这些linkId的声明。

问题1:我若替换掉了cameralink之后,这些后续的link必须也要去掉吧?

问题2:这些link仅仅针对sensor送出的数据产生作用吗?是不是capturelink根本不需要这些功能?

问题3:我所理解的isplink、vstablink这两个link的功能依次是缩放、稳像,而vnflink、mctnflink这两个link与nsflink又有什么区别?

问题4:valink的声明也是在cameraPrm中的,valink具体实现了什么功能?是否会影响我们最终capturelink前提下的va功能?